Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Polygon and Thermals issue
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 426 views
  • Users 0 members are here
  • polygons and thermals issue
Related

Polygon and Thermals issue

nikoly
nikoly over 10 years ago

Good Morning,

I have a 2 Layers PCB and I have to design a polygon (as the datasheet suggest) which surrounds three devices pad as you can see in the attached file (red rectangle).

 

I wonder if I can  set on the thermals without losing the benefits of polygon (as you can see the attached file ).

 

Setting on the thermals will give me an help for hand soldering but my fear is that I should lose the benefits of the polygon.

 

Sorry for this dummy question but I'm not an HW expert.

 

Hope you can help

Thanks a lotù

Nico

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 03.10.2016 08:34, nikk kik wrote:

    Good Morning,

    I have a 2 Layers PCB and I have to design a polygon (as the datasheet suggest) which surrounds three devices pad as you can see in the attached file (red rectangle).

     

    I wonder if I can  set on the thermals without losing the benefits of polygon (as you can see the attached file ).

     

    Yes thermals has some impact, but the effect is most likely negible. The

    resistance in the short thermal stubs are a small fraction compared to

    the full polygon. If there are 100's of amps peak, a few nanoohm may

    cause a non critical difference. Make sure the polygon wire is wide

    enough (looks ok on the img). You don't want very thin wires there.

     

    Note:This looks like a switch mode power supply circuit, and it looks

    like pin 5,6,7 should be connected with pin8? They seem to be missing.

    Make sure the pin to pad mapping in the device is the type that must

    connect all pins. Using only one of the pins will make a huge impact!

     

    Setting on the thermals will give me an help for hand soldering but my fear is that I should lose the benefits of the polygon.

     

    Wild guess, but you will probably get 99 of the 100% effect by doing

    this, wich is fine.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago

    On 03.10.2016 08:34, nikk kik wrote:

    Good Morning,

    I have a 2 Layers PCB and I have to design a polygon (as the datasheet suggest) which surrounds three devices pad as you can see in the attached file (red rectangle).

     

    I wonder if I can  set on the thermals without losing the benefits of polygon (as you can see the attached file ).

     

    Yes thermals has some impact, but the effect is most likely negible. The

    resistance in the short thermal stubs are a small fraction compared to

    the full polygon. If there are 100's of amps peak, a few nanoohm may

    cause a non critical difference. Make sure the polygon wire is wide

    enough (looks ok on the img). You don't want very thin wires there.

     

    Note:This looks like a switch mode power supply circuit, and it looks

    like pin 5,6,7 should be connected with pin8? They seem to be missing.

    Make sure the pin to pad mapping in the device is the type that must

    connect all pins. Using only one of the pins will make a huge impact!

     

    Setting on the thermals will give me an help for hand soldering but my fear is that I should lose the benefits of the polygon.

     

    Wild guess, but you will probably get 99 of the 100% effect by doing

    this, wich is fine.