EAGLE User Support (English) Polygon problem/bug.
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
  • Replies 14 replies
  • Subscribers 180 subscribers
  • Views 1460 views
  • Users 0 members are here
Related

Polygon problem/bug.

Joop14
Joop14 over 9 years ago

Dear Cadsoft team,

 

I created two polygons on the same layer. One covers the whole board and

has rank 1 and has thermals switched off.

The other polygon is smaller and has rank 2 and has thermals switched on.

 

The problem/bug is that the thermals on/off property is not taken into

account when checking the ranking of the two polygons. The thermals are

always switched off.

 

Could you fix this please?

 

Thanks.

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to Joop14

    Joop wrote:

     

    warrenbrayshaw wrote on Thu, 06 October 2016 20:07

    Well, working the way it does, gives me exactly what you described you

    needed. No thermals on SMD and thermals on pads. At least it works for

    me when I tried it using v7.2.2, before I wrote the reply.

    How about you make a small board to illustrate your problem and post it

    here with an image of what you see.

     

    Will do that. First I'll try with V7.7.

    It could be that this is a bug that has already been solved some time ago.

    I still use V6.22. We have the license for V7 but it's unusable slow with

    complex boards on our hardware.

     

    no need to reinvent the wheel 8-)

    just look at the example board file I posted earlier in this thread.

     

    thermals off is not overridden by thermal on, whereas thermal off over

    thermal on works as expected.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to Joop14

    On 7/10/2016 7:32 p.m., Joop wrote:

     

     

    I was mistaken. I am using V6.6, the last V6 version.

    Thanks anyway. I'll let you how it ends with the polygon test & V7.

     

     

    I tried it in v6.6 and it works fine there

    See attached board.

     

    One SMD and three pads are all connected to the same net as the two

    polygons. Turn off "Settings > Misc > Ratsnest processes polygons" to

    see the airwires.

     

    The polygons have the same name as the signal connected to those contacts.

    The outer Polygon is Rank 1 with thermals on

    THe inner is rank 2 with thermals off

     

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 9 years ago

    Thanks Warren.

     

    It works when I do it exactly the same way as you describe.

     

    The thing is, apart from a couple of connectors, all components are smd.

    So, I prefer to have the outer polygon which usually covers the whole

    board,

    set to thermals off. Then I want to draw two or three small polygons that

    cover

    only some throughole connectors with thermals set to on.

    This is the opposite of what you proposed and I can't get it to work.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to Joop14

    On 7/10/2016 10:34 p.m., Joop wrote:

    Thanks Warren.

     

    It works when I do it exactly the same way as you describe.

     

    The thing is, apart from a couple of connectors, all components are smd.

    So, I prefer to have the outer polygon which usually covers the whole

    board,

    set to thermals off. Then I want to draw two or three small polygons that

    cover

    only some throughole connectors with thermals set to on.

    This is the opposite of what you proposed and I can't get it to work.

     

     

    Hi

    There is a way to do it. See the attached

     

    The board sized outer GND polygon is made Rank 3, Thermals 'Off'.

     

    That makes the whole board, Thermals off and satisfies your SMDs.

     

    Next you thwart its efforts in the region of you connector with a

    polygon at Rank 2 with an Eagle generated signal name like S$7.

    Rank 2 is a higher ranking than the big polygon so the big polygon

    cannot go into that area. Hence there's a hole in the big polygon in the

    region of your connector.

     

    The you make another polygon a little larger than the last and give it

    Signal = GND,  Rank 1 , Thermals 'On'.

     

    Having a higher rank it wins and  suppresses the rank 2 polygon

    underneath it so the Rank 2 polygon becomes irrelevant but it's still

    doing its job holding the big rank 3 polygon at bay.

     

    With the RAnk1 polygon having  Thermals 'On', the connector pads have

    thermals as desired.

     

    Now there is an issue to be understood.

    Do a ratsnest and look in the spaces beside the traces. There's

    something there. It's the drawn outline of the unfilled Rank 2 polygon.

     

    This is a visual effect only in the CAD display.

    When you create your Gerber files, it is not there because the drawn

    polygon outline is not part of a Gerber. It is the calculated signal

    polygon that is conveyed to the Gerber.

    View the gerber to confirm this for yourself.

     

    I suspect, any print output from Eagle used to home-bake a board may

    show these display artefacts.  I did not check this.

     

    I understand many create the gerber and print that for their toner

    transfer or photo process.

     

    HTH

    Warren

     

     

     

     

     

     

    Attachments:
    poly_test_v6-6_3.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<