Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) create project from exist ing .sch and .brd files?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 1473 views
  • Users 0 members are here
Related

create project from exist ing .sch and .brd files?

gpsmikey
gpsmikey over 9 years ago

Greetings - clearly I am using the wrong keyword search - it must be a

simple process.  For example, on Github, there is a .sch and .brd file for

the Adafruit Huzzah board.  I can download the files, but I can't find the

incantation to create a project from the two files.  I can create a project

easily and I can copy the two files into the project folder, but the

project does not seem to know about the files.  It is easy to find info on

creating a new schematic in a project, but I have not been able to find how

to import the existing files into the project so it sees them.  (I have the

non-profit license).

 

Thanks!

Mike Fields

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Am 08.11.2016 um 03:40 schrieb Mike Fields:

    Adafruit Huzzah board

     

    That IS the project. image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 08.11.2016 08:18, Joern Paschedag wrote:

    Am 08.11.2016 um 03:40 schrieb Mike Fields:

    Adafruit Huzzah board

     

    That IS the project. image

     

    Not really.. You need an .epf file to really display the folder as a

    project in the control panel, but they do not have a strong dependancy.

     

    Usually when I download .brd and .sch files, I copy one of my .epf files

    from another project to the same folder. Only then, the folder will

    appear as a project folder in the control panel.

     

    Of course, when I open this project folder first time, it will try to

    open the last .sch and .brd used for the copied project, wich will be

    empty, but you can safely close them and click the brd or sch files in

    the project folder (while this project is open). Now the .epf will be

    tied to the downloaded .brd and .sch.

     

    Note, the .epf will remember certain parameters, like window positions,

    last opened .brd and .sch files, drill diameters used and such. Also

    note that some parameters get lost if you close a brd or sch while the

    project is open. This is an annoying side effect of the way "projects"

    are handled in Eagle.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 08.11.2016 08:18, Joern Paschedag wrote:

    Am 08.11.2016 um 03:40 schrieb Mike Fields:

    Adafruit Huzzah board

     

    That IS the project. image

     

    Not really.. You need an .epf file to really display the folder as a

    project in the control panel, but they do not have a strong dependancy.

     

    Usually when I download .brd and .sch files, I copy one of my .epf files

    from another project to the same folder. Only then, the folder will

    appear as a project folder in the control panel.

     

    Of course, when I open this project folder first time, it will try to

    open the last .sch and .brd used for the copied project, wich will be

    empty, but you can safely close them and click the brd or sch files in

    the project folder (while this project is open). Now the .epf will be

    tied to the downloaded .brd and .sch.

     

    Note, the .epf will remember certain parameters, like window positions,

    last opened .brd and .sch files, drill diameters used and such. Also

    note that some parameters get lost if you close a brd or sch while the

    project is open. This is an annoying side effect of the way "projects"

    are handled in Eagle.