Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Gateswap across schematic   sheets
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 187 subscribers
  • Views 2106 views
  • Users 0 members are here
Related

Gateswap across schematic   sheets

autodeskguest
autodeskguest over 9 years ago

I just discovered GATESWAP only works within the current schematic sheet.

I am using a quad opamp.  IC10A and IC10B are on schematic sheet 9, and

IC10C and IC10D on sheet 10.  Now that I'm placing parts on the board, I

want to swap IC10A <> IC10D and IC10B <> IC10C.

 

In the schematic editor, I went to sheet 9 and entered "gateswap ic10a

ic10d".  This resulted in the rather unhelpful pop "Can't swap gate IC10A

and IC10D".  Why can't these gates be swapped?  I checked the swaplevel of

each gate.  No, they are all set to 1.  Maybe the gate names need to be

enclosed in apostrophies?  No, that didn't help.  Upper case?  No, that

wasn't it either.

 

Then I tried "gateswap ic10a ic10b".  That worked.  OK, maybe I had a small

typo.  Using up-arrow, I got the previous command back and carefully

changed only the B to a D.  Now its back to "Can't swap gate IC10A and

IC10D".  It must be that gate A and D are on different sheets, but that's

not intuitive at all.

 

I got around this by moving all of the sheet 10 contents to the side of

sheet 9, doing the gateswaps, then moving the sheet 10 content back to

sheet 10.

 

Am I missing something?

 

If not, then here are my suggestions:Allow GATESWAP to work across

schematic sheets when entered as a command.

 

Fix the GATESWAP error dialog to explain why it can't swap the gates as

requested (incompatible swap level, different numbers of pins, no such

gate, not allowed on Tuesday afternoons, etc).

 

If you don't do #1, at least mention this limitation in the GATESWAP help

page.

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Olin Lathrop wrote:

    I just discovered GATESWAP only works within the current schematic sheet.

     

    It is clear why "gateswap (x1 y1) (x2 y2)" won't work across sheets

    (at least the clickety-click way, and the command line version would

    require an extended coordinate syntax), but ...

     

    ... I can't see any reason why "gateswap gate1 gate2" should pose any

    implementation problems.

     

     

    Disclaimer: I'm using 6.6, don't know if 7.x allows it.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 11/10/2016 2:17 AM, Lorenz wrote:

    Olin Lathrop wrote:

    I just discovered GATESWAP only works within the current schematic sheet.

     

    It is clear why "gateswap (x1 y1) (x2 y2)" won't work across sheets

    (at least the clickety-click way, and the command line version would

    require an extended coordinate syntax), but ...

     

    ... I can't see any reason why "gateswap gate1 gate2" should pose any

    implementation problems.

     

    Under the current Hierarchy implementation there is the possibility for

    ambiguity with the command line syntax.

     

    Disclaimer: I'm using 6.6, don't know if 7.x allows it.

    Just to clarify it still doesn't allow it.

     

    I'm of the opinion that a gateswap in the board would be most useful.

    Usually you decide to swap a gate because you are on the layout and

    realize using a different gate would simplify your routing task.

     

    The problem I see is that I can't think of what the user interface for

    that would be like. Now in current V7 we have to deal with how hierarchy

    is implemented and that confuses a lot of things.

     

    Do you guys have any ideas? If we can have a suggestion of what should

    be implemented then that gives direction for the devs. How would you

    guys want this to work?

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Jorge Garcia <jorge@cadsoftusa.com> wrote:

    On 11/10/2016 2:17 AM, Lorenz wrote:

    Olin Lathrop wrote:

    I just discovered GATESWAP only works within the current schematic sheet.

     

    It is clear why "gateswap (x1 y1) (x2 y2)" won't work across sheets

    (at least the clickety-click way, and the command line version would

    require an extended coordinate syntax), but ...

     

    ... I can't see any reason why "gateswap gate1 gate2" should pose any

    implementation problems.

     

    Under the current Hierarchy implementation there is the possibility for

    ambiguity with the command line syntax.

     

     

    I need to play more with multiple sheets before I understand that.

     

    I'm of the opinion that a gateswap in the board would be most useful.

    Usually you decide to swap a gate because you are on the layout and

    realize using a different gate would simplify your routing task.

     

    Agreed.

     

    The problem I see is that I can't think of what the user interface for

    that would be like. Now in current V7 we have to deal with how hierarchy

    is implemented and that confuses a lot of things.

     

    Do you guys have any ideas? If we can have a suggestion of what should

    be implemented then that gives direction for the devs. How would you

    guys want this to work?

     

    Definitely at the board layout level. Makes the most sense there

    from my perspective.

     

    For the board GUI interface, I humbly suggest

     

    1.  click on gate-swap. Would be nice to highlight device pins

    corresponding to swappable gates at this time - but the user knows

    which device anyway -- and it could get pretty crowded with many

    eligible devices;

     

    2. click on one gate pin and the other "eligible" pins are

    highlighted so that the user can easily see to select the

    (functionally) equivalent pin on another gate;

     

    3. click on one of the highlighted pins to finish and update the

    corresponding schematic.

     

    Finished.

     

    A different implementation would be to show the gate objects on the

    device at board level with connections and to let the user click and

    drag a gate objects to swap. But that changes the interface

    paradigm.  V10.1 perhaps. image

    --

    /"\ Bernd Felsche - Somewhere in Western Australia

    \ /  ASCII ribbon campaign | For every complex problem there is an

    X   against HTML mail     | answer that is clear, simple, and wrong.

    / \  and postings          |  --HL Mencken

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Jorge Garcia <jorge@cadsoftusa.com> wrote:

    On 11/10/2016 2:17 AM, Lorenz wrote:

    Olin Lathrop wrote:

    I just discovered GATESWAP only works within the current schematic sheet.

     

    It is clear why "gateswap (x1 y1) (x2 y2)" won't work across sheets

    (at least the clickety-click way, and the command line version would

    require an extended coordinate syntax), but ...

     

    ... I can't see any reason why "gateswap gate1 gate2" should pose any

    implementation problems.

     

    Under the current Hierarchy implementation there is the possibility for

    ambiguity with the command line syntax.

     

     

    I need to play more with multiple sheets before I understand that.

     

    I'm of the opinion that a gateswap in the board would be most useful.

    Usually you decide to swap a gate because you are on the layout and

    realize using a different gate would simplify your routing task.

     

    Agreed.

     

    The problem I see is that I can't think of what the user interface for

    that would be like. Now in current V7 we have to deal with how hierarchy

    is implemented and that confuses a lot of things.

     

    Do you guys have any ideas? If we can have a suggestion of what should

    be implemented then that gives direction for the devs. How would you

    guys want this to work?

     

    Definitely at the board layout level. Makes the most sense there

    from my perspective.

     

    For the board GUI interface, I humbly suggest

     

    1.  click on gate-swap. Would be nice to highlight device pins

    corresponding to swappable gates at this time - but the user knows

    which device anyway -- and it could get pretty crowded with many

    eligible devices;

     

    2. click on one gate pin and the other "eligible" pins are

    highlighted so that the user can easily see to select the

    (functionally) equivalent pin on another gate;

     

    3. click on one of the highlighted pins to finish and update the

    corresponding schematic.

     

    Finished.

     

    A different implementation would be to show the gate objects on the

    device at board level with connections and to let the user click and

    drag a gate objects to swap. But that changes the interface

    paradigm.  V10.1 perhaps. image

    --

    /"\ Bernd Felsche - Somewhere in Western Australia

    \ /  ASCII ribbon campaign | For every complex problem there is an

    X   against HTML mail     | answer that is clear, simple, and wrong.

    / \  and postings          |  --HL Mencken