Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Hole in stencil layer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 187 subscribers
  • Views 747 views
  • Users 0 members are here
Related

Hole in stencil layer

autodeskguest
autodeskguest over 9 years ago

Hello,

I have to provide a gerber file for stencil manufacturer house.

In the brd view I created a layer named "stencil" where I defined the

contour of the stencil. Then from CAM processor it's easy to add the

aperture from the cream layer(s).

 

I also need to add some hole for the SMT stencil printer.

These holes should be present only on the stencil gerber file, and not

in the PCB ones (they are outside the PCB of course).

 

Is there a convenient way to handle this?

I wouldn't create a second brd file just to add the holes...

 

Marco

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    On 11/17/2016 12:24 PM, Marco Trapanese wrote:

    Hello,

    I have to provide a gerber file for stencil manufacturer house.

    In the brd view I created a layer named "stencil" where I defined the

    contour of the stencil. Then from CAM processor it's easy to add the

    aperture from the cream layer(s).

     

    I also need to add some hole for the SMT stencil printer.

    These holes should be present only on the stencil gerber file, and not

    in the PCB ones (they are outside the PCB of course).

     

    Is there a convenient way to handle this?

    I wouldn't create a second brd file just to add the holes...

     

    Marco

     

    Hello Marco,

     

    I hope you're doing well. The easiest solution would be to draw a filled

    in circle on the stencil layer. Click the circle command, set the width

    to zero(this will make it fill).

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Il 17/11/2016 18:52, Jorge Garcia ha scritto:

     

    I hope you're doing well. The easiest solution would be to draw a filled

    in circle on the stencil layer. Click the circle command, set the width

    to zero(this will make it fill).

     

    This is a good hint!

    I bet I need to ask to the PCB house if they will recognize them as

    holes, actually.

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 18/11/2016 7:00 a.m., Marco Trapanese wrote:

    Il 17/11/2016 18:52, Jorge Garcia ha scritto:

     

    I hope you're doing well. The easiest solution would be to draw a filled

    in circle on the stencil layer. Click the circle command, set the width

    to zero(this will make it fill).

     

    This is a good hint!

    I bet I need to ask to the PCB house if they will recognize them as

    holes, actually.

     

     

     

     

     

    Hi Marco

     

    The PCB house should not recognise the filled circle is a hole. Your

    drill file specifies where holes go.

     

    If you are sending the eagle board file and not gerbers, they may

    calculate the board size as bigger because you have objects beyond the

    board edges. Hence the cost of the board may go up.

     

    That's what needs checking.

     

    If this is true there is a way around it using assembly variants.

    Make device that has a package with the filled circles on the stencil

    layer and a symbol you would like for the schematic. Then make these

    into simple device. Using assembly variants you essentially turn on and

    off those stencil holes because you turn off the device/package when set

    the assembly variant and save.

     

    You can do all this without a user defined stencil layer. Just use the

    cream layer

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 18/11/2016 7:00 a.m., Marco Trapanese wrote:

    Il 17/11/2016 18:52, Jorge Garcia ha scritto:

     

    I hope you're doing well. The easiest solution would be to draw a filled

    in circle on the stencil layer. Click the circle command, set the width

    to zero(this will make it fill).

     

    This is a good hint!

    I bet I need to ask to the PCB house if they will recognize them as

    holes, actually.

     

     

     

     

     

    Hi Marco

     

    The PCB house should not recognise the filled circle is a hole. Your

    drill file specifies where holes go.

     

    If you are sending the eagle board file and not gerbers, they may

    calculate the board size as bigger because you have objects beyond the

    board edges. Hence the cost of the board may go up.

     

    That's what needs checking.

     

    If this is true there is a way around it using assembly variants.

    Make device that has a package with the filled circles on the stencil

    layer and a symbol you would like for the schematic. Then make these

    into simple device. Using assembly variants you essentially turn on and

    off those stencil holes because you turn off the device/package when set

    the assembly variant and save.

     

    You can do all this without a user defined stencil layer. Just use the

    cream layer

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Il 17/11/2016 22:05, warrenbrayshaw ha scritto:

     

    If you are sending the eagle board file and not gerbers, they may

    calculate the board size as bigger because you have objects beyond the

    board edges. Hence the cost of the board may go up.

     

    I will send gerber file, not the EAGLE board one.

    And for stencil is a separate order, so I will upload only the stencil

    layer.

     

     

    If this is true there is a way around it using assembly variants.

    Make device that has a package with the filled circles on the stencil

    layer and a symbol you would like for the schematic. Then make these

    into simple device. Using assembly variants you essentially turn on and

    off those stencil holes because you turn off the device/package when set

    the assembly variant and save.

     

    You can do all this without a user defined stencil layer. Just use the

    cream layer

     

     

    If I understand correcly I need two variants. One with all components

    but the stencil one, and another with only the stencil.

     

    It might work! I'm going to give it a try.

    Thanks