Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How can I make Version 7 default in Windows 7?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 190 subscribers
  • Views 3120 views
  • Users 0 members are here
Related

How can I make Version 7 default in Windows 7?

autodeskguest
autodeskguest over 9 years ago

I am not an OS expert and maybe it shows image

 

Anyhow, because several clients of mine did not upgrade to V7 I must

also keep V6 on the computer. It rns Windows 7 64-bit Professional. Any

time I click on a *.sch file it opens it in V6. I cannot even select in

Windows to open in V7 because Eagle V7 doesn't show in the menu.

 

So far the only way to open such files is to fire up V7, then go through

the file open menues and open the file. Of course, this does not work

with an Eagle file attached to an email which will always open in V6.

 

What gives?

 

--

Regards, Joerg

 

http://www.analogconsultants.com/

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

    also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

    Good luck,

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-15 01:07, Tilmann Reh wrote:

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

      also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

     

    That is exactly what happens.

     

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 17/12/2016 4:28 a.m., Joerg wrote:

    On 2016-12-15 01:07, Tilmann Reh wrote:

     

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

     

    These are the words you need:

     

    In regedit:

    Navigate to Computer\HKEY_CLASSES_ROOT\Applications and find your .exe

    name. (eagle.exe)

     

    Navigate under its name to shell>open>command. In the 'Default' change

    its location to the actual location of the executable, is will look

    similar to this :

    "C:\Eagle7-7\bin\eagle.exe" "%1"

     

    Hit okay.

     

    You should not need to re-associate the file type but if you do you

    should see the eagle icon has changed as they are different by Eagle

    version.

     

    The above works for me.

    I have 5 versions of Eagle on my PC and I can change which version gets

    used by default for the associated file types.

     

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 17/12/2016 4:28 a.m., Joerg wrote:

    On 2016-12-15 01:07, Tilmann Reh wrote:

     

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

     

    These are the words you need:

     

    In regedit:

    Navigate to Computer\HKEY_CLASSES_ROOT\Applications and find your .exe

    name. (eagle.exe)

     

    Navigate under its name to shell>open>command. In the 'Default' change

    its location to the actual location of the executable, is will look

    similar to this :

    "C:\Eagle7-7\bin\eagle.exe" "%1"

     

    Hit okay.

     

    You should not need to re-associate the file type but if you do you

    should see the eagle icon has changed as they are different by Eagle

    version.

     

    The above works for me.

    I have 5 versions of Eagle on my PC and I can change which version gets

    used by default for the associated file types.

     

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-16 10:33, warrenbrayshaw wrote:

    On 17/12/2016 4:28 a.m., Joerg wrote:

    On 2016-12-15 01:07, Tilmann Reh wrote:

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

     

    These are the words you need:

     

    In regedit:

    Navigate to Computer\HKEY_CLASSES_ROOT\Applications and find your .exe

    name. (eagle.exe)

     

     

    The problem is, it's not there image

     

     

    Navigate under its name to shell>open>command. In the 'Default' change

    its location to the actual location of the executable, is will look

    similar to this :

    "C:\Eagle7-7\bin\eagle.exe" "%1"

     

    Hit okay.

     

    You should not need to re-associate the file type but if you do you

    should see the eagle icon has changed as they are different by Eagle

    version.

     

    The above works for me.

    I have 5 versions of Eagle on my PC and I can change which version gets

    used by default for the associated file types.

     

    Warren

     

     

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Am 17.12.2016 um 12:45 schrieb René König:

    Hi Joern!

     

    Am 17.12.2016 um 12:04 schrieb Joern Paschedag:

    But in the license agreement 1.2.1 of autodesk it reads that after an

    upgrade

    the "old" versions have to be uninstalled within 120 days after upgrade...

     

    With V6, you even had to replace previous versions immediately. But

    these 120 days made me curious, so I looked for the current EULA ... and

    could not find it. So where did you find that information?

     

    Rene

     

    Hi René,

    I started a setup for 7.7.0 and before installation one has to accept

    (or not) the license agreement.

    Click on the link and there you have it.

     

    I checked half morning for the EULA until I found on autodesk:

     

    http://www.autodesk.com/company/legal-notices-trademarks/software-license-agreements

     

    I couldn't find anything until I selected a language on that page.

    There is even one in german language but imo in case of differences only

    the english text counts.

    Typical lawyer stuff as usual.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Hi Joern!

     

    Am 17.12.2016 um 12:04 schrieb Joern Paschedag:

    But in the license agreement 1.2.1 of autodesk it reads that after an

    upgrade

    the "old" versions have to be uninstalled within 120 days after upgrade...

     

    With V6, you even had to replace previous versions immediately. But

    these 120 days made me curious, so I looked for the current EULA ... and

    could not find it. So where did you find that information?

     

    Rene

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Am 16.12.2016 um 19:33 schrieb warrenbrayshaw:

    On 17/12/2016 4:28 a.m., Joerg wrote:

    On 2016-12-15 01:07, Tilmann Reh wrote:

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

     

    These are the words you need:

     

    In regedit:

    Navigate to Computer\HKEY_CLASSES_ROOT\Applications and find your .exe

    name. (eagle.exe)

     

    Navigate under its name to shell>open>command. In the 'Default' change

    its location to the actual location of the executable, is will look

    similar to this :

    "C:\Eagle7-7\bin\eagle.exe" "%1"

     

    Hit okay.

     

    You should not need to re-associate the file type but if you do you

    should see the eagle icon has changed as they are different by Eagle

    version.

     

    The above works for me.

    I have 5 versions of Eagle on my PC and I can change which version gets

    used by default for the associated file types.

     

    Warren

     

     

    Hi Warren,

    I also have different versions of eagle installed because of some

    clients. No problem so far image

    But in the license agreement 1.2.1 of autodesk it reads that after an

    upgrade

    the "old" versions have to be uninstalled within 120 days after upgrade...

    This is not acceptable for me and so I shall not upgrade to Version 7.

    Or have I over read something?

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag