Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How can I make Version 7 default in Windows 7?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 190 subscribers
  • Views 3120 views
  • Users 0 members are here
Related

How can I make Version 7 default in Windows 7?

autodeskguest
autodeskguest over 9 years ago

I am not an OS expert and maybe it shows image

 

Anyhow, because several clients of mine did not upgrade to V7 I must

also keep V6 on the computer. It rns Windows 7 64-bit Professional. Any

time I click on a *.sch file it opens it in V6. I cannot even select in

Windows to open in V7 because Eagle V7 doesn't show in the menu.

 

So far the only way to open such files is to fire up V7, then go through

the file open menues and open the file. Of course, this does not work

with an Eagle file attached to an email which will always open in V6.

 

What gives?

 

--

Regards, Joerg

 

http://www.analogconsultants.com/

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

    also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

    Good luck,

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-15 01:07, Tilmann Reh wrote:

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

      also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

     

    That is exactly what happens.

     

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Am 16.12.2016 um 16:28 schrieb Joerg:

    On 2016-12-15 01:07, Tilmann Reh wrote:

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

      also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

     

    That is exactly what happens.

     

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

     

    Hi Joerg long time  no hear... image

     

    I too have clients who want modifications etc. in their "old" eagle

    versions.

    Generally I never install in the default partition (C:\) but into

    different hd partitions.

     

    On windows desktop I have the icons for the different versions of eagle

    and each pointing to the corresponding path by using the "-U" parameter.

    I didn't find it in "help" but finally found it in (version 5)

    \doc\update_en-txt:

     

      - The new command line option '-U' can be used to define the location

         of the 'eaglerc' file in which EAGLE stores user settings.

     

    Unfortunately  I didn't find much more about this parameter, but you can

    also change the name of the eaglerc-file ie. "eaglerc-512.usr":

     

    E:\EAGLE-5.12.0\bin\eagle.exe -U E:\Eagle-5.12.0\eaglerc-512.usr

     

    This means that my eagle is on drive E:\eagle-5.12.0 and the

    eaglerc(-512) file is in that directory too.

    This goes for other versions as well. Of course the paths must be set in

    the control panel too.

    It worked for me in all windows OS and now in win 8.1.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-18 04:36, Tilmann Reh wrote:

    Joerg schrieb:

     

    I want to keep the number of partions small. Programs go in C:\, data

    in E:\ and common info such as literature that doesn't need to be

    preotected in F:\.

     

    That's exactly the way I do. image

     

     

    Software should not require its own partition to run properly.

     

     

    On windows desktop I have the icons for the different versions of

    eagle and each pointing to the corresponding path by using the "-U"

    parameter. I didn't find it in "help" but finally found it in

    (version 5) \doc\update_en-txt:

     

    - The new command line option '-U' can be used to define the

    location of the 'eaglerc' file in which EAGLE stores user

    settings.

     

    Unfortunately  I didn't find much more about this parameter, but

    you can also change the name of the eaglerc-file ie.

    "eaglerc-512.usr":

     

    E:\EAGLE-5.12.0\bin\eagle.exe -U E:\Eagle-5.12.0\eaglerc-512.usr

     

    This means that my eagle is on drive E:\eagle-5.12.0 and the

    eaglerc(-512) file is in that directory too. This goes for other

    versions as well. Of course the paths must be set in the control

    panel too. It worked for me in all windows OS and now in win 8.1.

     

    That gets complicated. I think I'll just accept this Eagle-quirk for

    a while and thus have to store files first so I can open them from

    within Eagle instead of clicking on the file name. Not nice but at

    least that works.

     

    When running different versions of EAGLE at the same computer you need

    to use different eaglerc.usr files anyway that point to different

    folders with libraries, projects etc.

     

    However, this is not related to the original question. image

     

    Anyway, with EAGLEs really weird control panel and the lack of support

    for ambiguously located and named projewct files, it's best to first

    start EAGLE and then select projects and files from there.

     

    I also work file-oriented with all my tools - except for EAGLE. :-\

     

     

    In some user-friendliness aspects Eagle is stuck in the 20th century.

    However, I have to say that it is very robust software. Unlike Orcad it

    has never crashed running on Windows XP. On Windows 7 64-bit it does

    crash but only rarely, not to an extent where it impedes my work.

     

    I am surprised how many companies here in the US are using Eagle by now,

    especially small ones where innovation mostly happens.

     

    Back to the bowl of brandy beans now ... :-0

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Joerg schrieb:

     

    I want to keep the number of partions small. Programs go in C:\, data

    in E:\ and common info such as literature that doesn't need to be

    preotected in F:\.

     

    That's exactly the way I do. image

     

    On windows desktop I have the icons for the different versions of

    eagle and each pointing to the corresponding path by using the "-U"

    parameter. I didn't find it in "help" but finally found it in

    (version 5) \doc\update_en-txt:

     

    - The new command line option '-U' can be used to define the

    location of the 'eaglerc' file in which EAGLE stores user

    settings.

     

    Unfortunately  I didn't find much more about this parameter, but

    you can also change the name of the eaglerc-file ie.

    "eaglerc-512.usr":

     

    E:\EAGLE-5.12.0\bin\eagle.exe -U E:\Eagle-5.12.0\eaglerc-512.usr

     

    This means that my eagle is on drive E:\eagle-5.12.0 and the

    eaglerc(-512) file is in that directory too. This goes for other

    versions as well. Of course the paths must be set in the control

    panel too. It worked for me in all windows OS and now in win 8.1.

     

    That gets complicated. I think I'll just accept this Eagle-quirk for

    a while and thus have to store files first so I can open them from

    within Eagle instead of clicking on the file name. Not nice but at

    least that works.

     

    When running different versions of EAGLE at the same computer you need

    to use different eaglerc.usr files anyway that point to different

    folders with libraries, projects etc.

     

    However, this is not related to the original question. image

     

    Anyway, with EAGLEs really weird control panel and the lack of support

    for ambiguously located and named projewct files, it's best to first

    start EAGLE and then select projects and files from there.

     

    I also work file-oriented with all my tools - except for EAGLE. :-\

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Joerg schrieb:

     

    I want to keep the number of partions small. Programs go in C:\, data

    in E:\ and common info such as literature that doesn't need to be

    preotected in F:\.

     

    That's exactly the way I do. image

     

    On windows desktop I have the icons for the different versions of

    eagle and each pointing to the corresponding path by using the "-U"

    parameter. I didn't find it in "help" but finally found it in

    (version 5) \doc\update_en-txt:

     

    - The new command line option '-U' can be used to define the

    location of the 'eaglerc' file in which EAGLE stores user

    settings.

     

    Unfortunately  I didn't find much more about this parameter, but

    you can also change the name of the eaglerc-file ie.

    "eaglerc-512.usr":

     

    E:\EAGLE-5.12.0\bin\eagle.exe -U E:\Eagle-5.12.0\eaglerc-512.usr

     

    This means that my eagle is on drive E:\eagle-5.12.0 and the

    eaglerc(-512) file is in that directory too. This goes for other

    versions as well. Of course the paths must be set in the control

    panel too. It worked for me in all windows OS and now in win 8.1.

     

    That gets complicated. I think I'll just accept this Eagle-quirk for

    a while and thus have to store files first so I can open them from

    within Eagle instead of clicking on the file name. Not nice but at

    least that works.

     

    When running different versions of EAGLE at the same computer you need

    to use different eaglerc.usr files anyway that point to different

    folders with libraries, projects etc.

     

    However, this is not related to the original question. image

     

    Anyway, with EAGLEs really weird control panel and the lack of support

    for ambiguously located and named projewct files, it's best to first

    start EAGLE and then select projects and files from there.

     

    I also work file-oriented with all my tools - except for EAGLE. :-\

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-18 04:36, Tilmann Reh wrote:

    Joerg schrieb:

     

    I want to keep the number of partions small. Programs go in C:\, data

    in E:\ and common info such as literature that doesn't need to be

    preotected in F:\.

     

    That's exactly the way I do. image

     

     

    Software should not require its own partition to run properly.

     

     

    On windows desktop I have the icons for the different versions of

    eagle and each pointing to the corresponding path by using the "-U"

    parameter. I didn't find it in "help" but finally found it in

    (version 5) \doc\update_en-txt:

     

    - The new command line option '-U' can be used to define the

    location of the 'eaglerc' file in which EAGLE stores user

    settings.

     

    Unfortunately  I didn't find much more about this parameter, but

    you can also change the name of the eaglerc-file ie.

    "eaglerc-512.usr":

     

    E:\EAGLE-5.12.0\bin\eagle.exe -U E:\Eagle-5.12.0\eaglerc-512.usr

     

    This means that my eagle is on drive E:\eagle-5.12.0 and the

    eaglerc(-512) file is in that directory too. This goes for other

    versions as well. Of course the paths must be set in the control

    panel too. It worked for me in all windows OS and now in win 8.1.

     

    That gets complicated. I think I'll just accept this Eagle-quirk for

    a while and thus have to store files first so I can open them from

    within Eagle instead of clicking on the file name. Not nice but at

    least that works.

     

    When running different versions of EAGLE at the same computer you need

    to use different eaglerc.usr files anyway that point to different

    folders with libraries, projects etc.

     

    However, this is not related to the original question. image

     

    Anyway, with EAGLEs really weird control panel and the lack of support

    for ambiguously located and named projewct files, it's best to first

    start EAGLE and then select projects and files from there.

     

    I also work file-oriented with all my tools - except for EAGLE. :-\

     

     

    In some user-friendliness aspects Eagle is stuck in the 20th century.

    However, I have to say that it is very robust software. Unlike Orcad it

    has never crashed running on Windows XP. On Windows 7 64-bit it does

    crash but only rarely, not to an extent where it impedes my work.

     

    I am surprised how many companies here in the US are using Eagle by now,

    especially small ones where innovation mostly happens.

     

    Back to the bowl of brandy beans now ... :-0

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/