Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How can I make Version 7 default in Windows 7?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 190 subscribers
  • Views 3118 views
  • Users 0 members are here
Related

How can I make Version 7 default in Windows 7?

autodeskguest
autodeskguest over 9 years ago

I am not an OS expert and maybe it shows image

 

Anyhow, because several clients of mine did not upgrade to V7 I must

also keep V6 on the computer. It rns Windows 7 64-bit Professional. Any

time I click on a *.sch file it opens it in V6. I cannot even select in

Windows to open in V7 because Eagle V7 doesn't show in the menu.

 

So far the only way to open such files is to fire up V7, then go through

the file open menues and open the file. Of course, this does not work

with an Eagle file attached to an email which will always open in V6.

 

What gives?

 

--

Regards, Joerg

 

http://www.analogconsultants.com/

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Am 16.12.2016 um 16:28 schrieb Joerg:

    On 2016-12-15 01:07, Tilmann Reh wrote:

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

      also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

     

    That is exactly what happens.

     

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

     

    Hi Joerg long time  no hear... image

     

    I too have clients who want modifications etc. in their "old" eagle

    versions.

    Generally I never install in the default partition (C:\) but into

    different hd partitions.

     

    On windows desktop I have the icons for the different versions of eagle

    and each pointing to the corresponding path by using the "-U" parameter.

    I didn't find it in "help" but finally found it in (version 5)

    \doc\update_en-txt:

     

      - The new command line option '-U' can be used to define the location

         of the 'eaglerc' file in which EAGLE stores user settings.

     

    Unfortunately  I didn't find much more about this parameter, but you can

    also change the name of the eaglerc-file ie. "eaglerc-512.usr":

     

    E:\EAGLE-5.12.0\bin\eagle.exe -U E:\Eagle-5.12.0\eaglerc-512.usr

     

    This means that my eagle is on drive E:\eagle-5.12.0 and the

    eaglerc(-512) file is in that directory too.

    This goes for other versions as well. Of course the paths must be set in

    the control panel too.

    It worked for me in all windows OS and now in win 8.1.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 17/12/2016 4:28 a.m., Joerg wrote:

    On 2016-12-15 01:07, Tilmann Reh wrote:

     

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

     

    These are the words you need:

     

    In regedit:

    Navigate to Computer\HKEY_CLASSES_ROOT\Applications and find your .exe

    name. (eagle.exe)

     

    Navigate under its name to shell>open>command. In the 'Default' change

    its location to the actual location of the executable, is will look

    similar to this :

    "C:\Eagle7-7\bin\eagle.exe" "%1"

     

    Hit okay.

     

    You should not need to re-associate the file type but if you do you

    should see the eagle icon has changed as they are different by Eagle

    version.

     

    The above works for me.

    I have 5 versions of Eagle on my PC and I can change which version gets

    used by default for the associated file types.

     

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to zainka

    On 2016-12-14 15:33, vidar vidnes wrote:

    May-bee I have misunderstood the problem here but Eagle 7 does not

    (or did not fro me, more correctly) install to program files, but it

    ended up directly on the root, at c:\ So right click on the schematic

    file, choose "open with...", make sure the "Always use the

    selected...." checkbox is selected and then browse manually to the

    bin file and select the file named eagle (remember that in later

    windows the extension does not always show). Check c:\ for an eagle

    folder.

     

     

    V7 installed correctly in the 64-bit section. I think Tilmann has

    diagnosed the problem correctly. The fix requires a registry edit

    though. Not for the faint of heart and I'll do that during a quiet phase

    in case I brick the PC.

     

    In case an engineer from Eagle is reading: This should be fixed.

    Independent engineers such as consultants have to be able to run older

    versions because not all their clients have the latest version.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-15 01:07, Tilmann Reh wrote:

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

      also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

     

    That is exactly what happens.

     

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

     

    Registry edits are risk business, like walking close to the edge of a

    cliff. Thanks for the hint. I'll tackle that next year, or try, when

    there is time in case I need to unbrick the computer. Got a surprise

    project that has to be done by end of December. However, since I still

    have to wait for the specs I am going to brew beer today image

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

    also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

    Good luck,

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • zainka
    zainka over 9 years ago in reply to autodeskguest

    May-bee I have misunderstood the problem here but Eagle 7 does not (or did not fro me, more correctly) install to program files, but it ended up directly on the root, at c:\

    So right click on the schematic file, choose "open with...", make sure the "Always use the selected...." checkbox is selected and then browse manually to the bin folder and select the file named eagle (remember that in later windows the extension does not always show). Check c:\ for an eagle folder.

     

     

     

     

    EDIT: Fixed an typo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-14 14:22, René König wrote:

    Am 14.12.2016 um 21:12 schrieb Joerg:

    I know where it runs, in Program Files\Eagle7.2.0\bin. However, that

    will not show up under browse. Only the V6 location does.

     

    V6 should show up below "Program Files(x86)", not "Program Files". Are

    you sure that you looked up the correct directory?

     

     

     

    Yes, V6 must be and is in the (x86) directory but not V7. The problem is

    that V7 never shows up in any default program selections. So I can't

    tell Windows to always use that as the default for *.sch files. That can

    make a real mess if I don't notice it and work on libraries.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Am 14.12.2016 um 21:12 schrieb Joerg:

    I know where it runs, in Program Files\Eagle7.2.0\bin. However, that

    will not show up under browse. Only the V6 location does.

     

    V6 should show up below "Program Files(x86)", not "Program Files". Are

    you sure that you looked up the correct directory?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to clem57

    On 2016-12-14 09:50, Clem Martins wrote:

    click Browse to find the program you want to use, and then click

    Open. If no other programs are installed that are able to open the

    file type or protocol, your choices will be limited.)

    The key is to look at shortcut to find where the program was

    installed to. Once that is known, the browse will allow you to follow

    the same paths to that program. Clem

     

     

    I know where it runs, in Program Files\Eagle7.2.0\bin. However, that

    will not show up under browse. Only the V6 location does.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to autodeskguest

    click Browse to find the program you want to use, and then click Open. If no other programs are installed that are able to open the file type or protocol, your choices will be limited.)

    The key is to look at shortcut to find where the program was installed to. Once that is known, the browse will allow you to follow the same paths to that program.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>