EAGLE User Support (English) How can I make Version 7 default in Windows 7?
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
  • Replies 24 replies
  • Subscribers 182 subscribers
  • Views 2618 views
  • Users 0 members are here
Related

How can I make Version 7 default in Windows 7?

autodeskguest
autodeskguest over 9 years ago

I am not an OS expert and maybe it shows image

 

Anyhow, because several clients of mine did not upgrade to V7 I must

also keep V6 on the computer. It rns Windows 7 64-bit Professional. Any

time I click on a *.sch file it opens it in V6. I cannot even select in

Windows to open in V7 because Eagle V7 doesn't show in the menu.

 

So far the only way to open such files is to fire up V7, then go through

the file open menues and open the file. Of course, this does not work

with an Eagle file attached to an email which will always open in V6.

 

What gives?

 

--

Regards, Joerg

 

http://www.analogconsultants.com/

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 9 years ago

    Hi Joerg,

     

    right click the file in question, choose "Open with" -> "Select default

    program". Everything you need is here, including the "Browse" button on

    the lower right corner.

     

    The actual wording might be different, though. My installation does not

    show up in english.

     

    Rene

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago

    https://support.microsoft.com/en-us/help/18539/windows-7-change-default-programs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-13 16:11, René König wrote:

    Hi Joerg,

     

    right click the file in question, choose "Open with" -> "Select default

    program". Everything you need is here, including the "Browse" button on

    the lower right corner.

     

     

    But Eagle V7 does not show up when you do that, only V6, and that's my

    problem.

     

     

    The actual wording might be different, though. My installation does not

    show up in english.

     

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to clem57

    On 2016-12-13 21:08, Clem Martins wrote:

    https://support.microsoft.com/en-us/help/18539/windows-7-change-default-programs

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/211114

     

     

    As I wrote, that only shows "eagle.exe" and this results in V6 being

    opened. V7 does not show up. V7 can only be opened direcvtly or via the

    desktop shortcut.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to autodeskguest

    click Browse to find the program you want to use, and then click Open. If no other programs are installed that are able to open the file type or protocol, your choices will be limited.)

    The key is to look at shortcut to find where the program was installed to. Once that is known, the browse will allow you to follow the same paths to that program.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to clem57

    On 2016-12-14 09:50, Clem Martins wrote:

    click Browse to find the program you want to use, and then click

    Open. If no other programs are installed that are able to open the

    file type or protocol, your choices will be limited.)

    The key is to look at shortcut to find where the program was

    installed to. Once that is known, the browse will allow you to follow

    the same paths to that program. Clem

     

     

    I know where it runs, in Program Files\Eagle7.2.0\bin. However, that

    will not show up under browse. Only the V6 location does.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Am 14.12.2016 um 21:12 schrieb Joerg:

    I know where it runs, in Program Files\Eagle7.2.0\bin. However, that

    will not show up under browse. Only the V6 location does.

     

    V6 should show up below "Program Files(x86)", not "Program Files". Are

    you sure that you looked up the correct directory?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 2016-12-14 14:22, René König wrote:

    Am 14.12.2016 um 21:12 schrieb Joerg:

    I know where it runs, in Program Files\Eagle7.2.0\bin. However, that

    will not show up under browse. Only the V6 location does.

     

    V6 should show up below "Program Files(x86)", not "Program Files". Are

    you sure that you looked up the correct directory?

     

     

     

    Yes, V6 must be and is in the (x86) directory but not V7. The problem is

    that V7 never shows up in any default program selections. So I can't

    tell Windows to always use that as the default for *.sch files. That can

    make a real mess if I don't notice it and work on libraries.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • zainka
    zainka over 9 years ago in reply to autodeskguest

    May-bee I have misunderstood the problem here but Eagle 7 does not (or did not fro me, more correctly) install to program files, but it ended up directly on the root, at c:\

    So right click on the schematic file, choose "open with...", make sure the "Always use the selected...." checkbox is selected and then browse manually to the bin folder and select the file named eagle (remember that in later windows the extension does not always show). Check c:\ for an eagle folder.

     

     

     

     

    EDIT: Fixed an typo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago

    Joerg schrieb:

     

    I am not an OS expert and maybe it shows image

     

    Anyhow, because several clients of mine did not upgrade to V7 I must

    also keep V6 on the computer. It rns Windows 7 64-bit Professional.

    Any time I click on a *.sch file it opens it in V6. I cannot even

    select in Windows to open in V7 because Eagle V7 doesn't show in the

    menu.

     

    So far the only way to open such files is to fire up V7, then go

    through the file open menues and open the file. Of course, this does

    not work with an Eagle file attached to an email which will always

    open in V6.

     

    What gives?

     

    Hello Joerg,

     

    welcome back here. image

     

    I vaguely remember having had about the same problem. In the selection

    dialog for the "standard program", only "EAGLE" is shown - without any

    version information, and so you can't tell which version to use. Even

    worse, even if you explicitly select the path to a particular version,

    windows will later still use the previous default.

     

    AFAIK, the cause for this problem are the registry entries that EAGLE

    creates during installation. The "program name" (or so) is set

    identically for all versions of EAGLE, and windows just picks the first

    match when setting the "standard", regardless of the (manually and

    explicitly) given path.

     

    I think I changed the values in the registry manually so they were

    different... Not perfectly sure, however - it's been some time ago...

     

    Good luck,

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>