Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) EAGLE v8.0 Implicit Group   Command (Yeh) and Beeps on Every Left-Button Click (Boo)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 191 subscribers
  • Views 2862 views
  • Users 0 members are here
Related

EAGLE v8.0 Implicit Group   Command (Yeh) and Beeps on Every Left-Button Click (Boo)

autodeskguest
autodeskguest over 9 years ago

Trying to keep an open mind about v8.0 and hoping that the licensing issues

will work themselves out....

 

For for now, seeing what's different.  First thing I noticed is that EAGLE

finally has implicit grouping.  I suggested this years ago and finally it's

made it in.  Basically, if you don't have a command active and you draw a

rectangle it will create an EAGLE group as if you ran the EAGLE group

command (not persistent groups like other CAD software has, but essentially

a temporary group for the next command, like EAGLE has always had).

 

So that is great.  That will save lots of mouse clicks once I get used to

it.

 

But.....

 

Now I get an error beep on the first left-mouse button click whenever a

command isn't active, including the first corner of a group.  That is super

annoying.  For instance, in the schematic editor, a left-click anywhere

(with no command active) will beep AND start creating the first line in a

polygon for creating a group.  Very similar in PCB editor.

 

Also, when I run the group command I get a beep on the first mouse click

even when EAGLE should know that clicking in an area with no objects is

actually expected.

 

I assume that this is maybe something that somehow got missed (maybe the

sound was down) when implementing the implicit group function.  But it

should be fixed as it is really annoying.

 

Cheers,

 

James.

--

James Morrison  ~~~  Stratford Digital

http://www.stratforddigital.ca

--

http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

 

  • Sign in to reply
  • Cancel
Parents
  • axnfell
    axnfell over 9 years ago

    I just cannot believe that something so simple is not implemented in the software, in EVERY package that I have used over the years you just have to left click and hold down the mouse button, draw and area over the objects you wish to move and then just release the mouse and then just drag it to where you want it to be, in fact the same procedure is available in well over 90% of ANY applications available in Windows and Mac OSX, I was asked to convert a load of schematics into eagle format for a client, after trying to get eagle to at least operate as a normal piece of software for 2 weeks now I have never been so frustrated, and cannot understand why this software is rated so highly especially when even simple tasks are stupidly problematic, I certainly cannot see our company purchasing a subscription to a piece of software that is basically unusable to the point where something I can do in Labcenter Proteus, Altium or PADs in a second, now takes ages to do in Eagle and sometimes just even then doesn't work as it should.

     

    The beeps are annoying and thanks for the help to turn these off, but a simple task of moving groups of objects around the screen, is just too pathetic to warrant spending money on software that is not even productive.

     

    Thanks for the help, but from searching the web it seems that Cadsoft never thought that fixing this was worth doing, and I have seen what Autodesk do to good software in the past so I certainly cannot see it being fixed soon or even ever...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • axnfell
    axnfell over 9 years ago

    I just cannot believe that something so simple is not implemented in the software, in EVERY package that I have used over the years you just have to left click and hold down the mouse button, draw and area over the objects you wish to move and then just release the mouse and then just drag it to where you want it to be, in fact the same procedure is available in well over 90% of ANY applications available in Windows and Mac OSX, I was asked to convert a load of schematics into eagle format for a client, after trying to get eagle to at least operate as a normal piece of software for 2 weeks now I have never been so frustrated, and cannot understand why this software is rated so highly especially when even simple tasks are stupidly problematic, I certainly cannot see our company purchasing a subscription to a piece of software that is basically unusable to the point where something I can do in Labcenter Proteus, Altium or PADs in a second, now takes ages to do in Eagle and sometimes just even then doesn't work as it should.

     

    The beeps are annoying and thanks for the help to turn these off, but a simple task of moving groups of objects around the screen, is just too pathetic to warrant spending money on software that is not even productive.

     

    Thanks for the help, but from searching the web it seems that Cadsoft never thought that fixing this was worth doing, and I have seen what Autodesk do to good software in the past so I certainly cannot see it being fixed soon or even ever...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rachaelp
    rachaelp over 9 years ago in reply to axnfell

    James Sawle wrote:

     

    I just cannot believe that something so simple is not implemented in the software, in EVERY package that I have used over the years you just have to left click and hold down the mouse button, draw and area over the objects you wish to move and then just release the mouse and then just drag it to where you want it to be, in fact the same procedure is available in well over 90% of ANY applications available in Windows and Mac OSX, I was asked to convert a load of schematics into eagle format for a client, after trying to get eagle to at least operate as a normal piece of software for 2 weeks now I have never been so frustrated, and cannot understand why this software is rated so highly especially when even simple tasks are stupidly problematic, I certainly cannot see our company purchasing a subscription to a piece of software that is basically unusable to the point where something I can do in Labcenter Proteus, Altium or PADs in a second, now takes ages to do in Eagle and sometimes just even then doesn't work as it should.

     

    The beeps are annoying and thanks for the help to turn these off, but a simple task of moving groups of objects around the screen, is just too pathetic to warrant spending money on software that is not even productive.

     

    Thanks for the help, but from searching the web it seems that Cadsoft never thought that fixing this was worth doing, and I have seen what Autodesk do to good software in the past so I certainly cannot see it being fixed soon or even ever...

    It is implemented in EAGLE. The latest "Group mode always on" change in v8 makes EAGLE do exactly as you wish. It just has a bug for some reason in this version v8.0.2 for some people which makes it not behave quite right but I know they are working on fixing it.

     

    But even without this change EAGLE is certainly not unusable and to claim it takes far longer to do things than other packages isn't accurate. FYI, I also use DxDesigner/PADS regularly and to me EAGLE is far quicker to do a lot of tasks. You just need to learn how to use it which really doesn't take that long. There are loads of tutorials around which can get you working efficiently quite quickly and if you don't know how to do something then just ask, there are usually plenty of people around who will be willing to help.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Ritchie75
    Ritchie75 over 9 years ago in reply to axnfell

    It is the problem with this software, simple things are not implemented, while it is full of very complex functions

     

    I maintain that the graphic edition of the components deserve to be simplified, to edit a component or Import a Logo it sometimes takes hours, gentlemen from CADSOFT it is in 2017 !!!!, you can not put some function of Abode Illustrator in the graphic part? Otherwise it is a very good software ...

     

    What a pity !!

     

    Ritchie