Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) EAGLE v8.0 Implicit Group   Command (Yeh) and Beeps on Every Left-Button Click (Boo)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 191 subscribers
  • Views 2862 views
  • Users 0 members are here
Related

EAGLE v8.0 Implicit Group   Command (Yeh) and Beeps on Every Left-Button Click (Boo)

autodeskguest
autodeskguest over 9 years ago

Trying to keep an open mind about v8.0 and hoping that the licensing issues

will work themselves out....

 

For for now, seeing what's different.  First thing I noticed is that EAGLE

finally has implicit grouping.  I suggested this years ago and finally it's

made it in.  Basically, if you don't have a command active and you draw a

rectangle it will create an EAGLE group as if you ran the EAGLE group

command (not persistent groups like other CAD software has, but essentially

a temporary group for the next command, like EAGLE has always had).

 

So that is great.  That will save lots of mouse clicks once I get used to

it.

 

But.....

 

Now I get an error beep on the first left-mouse button click whenever a

command isn't active, including the first corner of a group.  That is super

annoying.  For instance, in the schematic editor, a left-click anywhere

(with no command active) will beep AND start creating the first line in a

polygon for creating a group.  Very similar in PCB editor.

 

Also, when I run the group command I get a beep on the first mouse click

even when EAGLE should know that clicking in an area with no objects is

actually expected.

 

I assume that this is maybe something that somehow got missed (maybe the

sound was down) when implementing the implicit group function.  But it

should be fixed as it is really annoying.

 

Cheers,

 

James.

--

James Morrison  ~~~  Stratford Digital

http://www.stratforddigital.ca

--

http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

 

  • Sign in to reply
  • Cancel
Parents
  • axnfell
    axnfell over 9 years ago

    I just cannot believe that something so simple is not implemented in the software, in EVERY package that I have used over the years you just have to left click and hold down the mouse button, draw and area over the objects you wish to move and then just release the mouse and then just drag it to where you want it to be, in fact the same procedure is available in well over 90% of ANY applications available in Windows and Mac OSX, I was asked to convert a load of schematics into eagle format for a client, after trying to get eagle to at least operate as a normal piece of software for 2 weeks now I have never been so frustrated, and cannot understand why this software is rated so highly especially when even simple tasks are stupidly problematic, I certainly cannot see our company purchasing a subscription to a piece of software that is basically unusable to the point where something I can do in Labcenter Proteus, Altium or PADs in a second, now takes ages to do in Eagle and sometimes just even then doesn't work as it should.

     

    The beeps are annoying and thanks for the help to turn these off, but a simple task of moving groups of objects around the screen, is just too pathetic to warrant spending money on software that is not even productive.

     

    Thanks for the help, but from searching the web it seems that Cadsoft never thought that fixing this was worth doing, and I have seen what Autodesk do to good software in the past so I certainly cannot see it being fixed soon or even ever...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to axnfell

    James Sawle wrote:

     

    I just cannot believe that something so simple is not implemented in the software, in EVERY package that I have used over the years you just have to left click and hold down the mouse button, draw and area over the objects you wish to move and then just release the mouse and then just drag it to where you want it to be, in fact the same procedure is available in well over 90% of ANY applications available in Windows and Mac OSX, I was asked to convert a load of schematics into eagle format for a client, after trying to get eagle to at least operate as a normal piece of software for 2 weeks now I have never been so frustrated, and cannot understand why this software is rated so highly especially when even simple tasks are stupidly problematic, I certainly cannot see our company purchasing a subscription to a piece of software that is basically unusable to the point where something I can do in Labcenter Proteus, Altium or PADs in a second, now takes ages to do in Eagle and sometimes just even then doesn't work as it should.

     

    The beeps are annoying and thanks for the help to turn these off, but a simple task of moving groups of objects around the screen, is just too pathetic to warrant spending money on software that is not even productive.

     

    Thanks for the help, but from searching the web it seems that Cadsoft never thought that fixing this was worth doing, and I have seen what Autodesk do to good software in the past so I certainly cannot see it being fixed soon or even ever...

    It is implemented in EAGLE. The latest "Group mode always on" change in v8 makes EAGLE do exactly as you wish. It just has a bug for some reason in this version v8.0.2 for some people which makes it not behave quite right but I know they are working on fixing it.

     

    But even without this change EAGLE is certainly not unusable and to claim it takes far longer to do things than other packages isn't accurate. FYI, I also use DxDesigner/PADS regularly and to me EAGLE is far quicker to do a lot of tasks. You just need to learn how to use it which really doesn't take that long. There are loads of tutorials around which can get you working efficiently quite quickly and if you don't know how to do something then just ask, there are usually plenty of people around who will be willing to help.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago in reply to axnfell

    James Sawle wrote:

     

    I just cannot believe that something so simple is not implemented in the software, in EVERY package that I have used over the years you just have to left click and hold down the mouse button, draw and area over the objects you wish to move and then just release the mouse and then just drag it to where you want it to be, in fact the same procedure is available in well over 90% of ANY applications available in Windows and Mac OSX, I was asked to convert a load of schematics into eagle format for a client, after trying to get eagle to at least operate as a normal piece of software for 2 weeks now I have never been so frustrated, and cannot understand why this software is rated so highly especially when even simple tasks are stupidly problematic, I certainly cannot see our company purchasing a subscription to a piece of software that is basically unusable to the point where something I can do in Labcenter Proteus, Altium or PADs in a second, now takes ages to do in Eagle and sometimes just even then doesn't work as it should.

     

    The beeps are annoying and thanks for the help to turn these off, but a simple task of moving groups of objects around the screen, is just too pathetic to warrant spending money on software that is not even productive.

     

    Thanks for the help, but from searching the web it seems that Cadsoft never thought that fixing this was worth doing, and I have seen what Autodesk do to good software in the past so I certainly cannot see it being fixed soon or even ever...

    It is implemented in EAGLE. The latest "Group mode always on" change in v8 makes EAGLE do exactly as you wish. It just has a bug for some reason in this version v8.0.2 for some people which makes it not behave quite right but I know they are working on fixing it.

     

    But even without this change EAGLE is certainly not unusable and to claim it takes far longer to do things than other packages isn't accurate. FYI, I also use DxDesigner/PADS regularly and to me EAGLE is far quicker to do a lot of tasks. You just need to learn how to use it which really doesn't take that long. There are loads of tutorials around which can get you working efficiently quite quickly and if you don't know how to do something then just ask, there are usually plenty of people around who will be willing to help.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rachaelp
    rachaelp over 9 years ago in reply to COMPACT

    COMPACT wrote:

     

    Silly me!

    My PC was outputting sound to a non existent HDMI speakers.

    Yes it does beep for the initial group click - that doesn't annoy me because I'm accustomed to it.

    May be a workaround is to mute the speaker.

    No need to mute the speaker, you can turn the beep off in the settings.

    COMPACT wrote:

     

    It appears that most of you haven't read my Design Challenge posts which mention that to use EAGLE successfully you have to rewire your thinking to match the logic of its original designers.

    It's not dissimilar to German cars where you turn on a switch to turn on a light that which indicates that you've turned off the Air Conditioning.

    The designers appear to use the same core libraries for each all of the modules (PCB, Schematic and Library Manager) to make them very efficient which explains why some actions don't necessarily match the operator's assumptions and also have made the program platform agnostic (pc, mac, Linux). It can be infuriating at first but once you've adapted and become accustomed it works very well.

    Agreed. I think as soon as you understand that the UI is simply a front end for the command line commands then reading and understanding how they work makes it all fall into place. It did for me anyway.

    COMPACT wrote:

     

    One big gotcha is that the default configuration EAGLE assumes that the user has a 3 button mouse - with the middle button used panning the current view.

    For one of my mice it's the scroll wheel button.

     

    Another gotcha for the Schematic Editor is to place Nets and not Lines. The Net tool differs from the normal Line tool by performing the extras required for net management.

    If you have used lines inadvertently they can bite you on your proverbials later on.

    Useful tips for people new to EAGLE. On the subject of the mouse, before v8 it was a little awkward on a Mac to change routing layer as the mac doesn't have a middle button! This has at least been fixed in v8 :-)

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to rachaelp

    Silly me!

    My PC was outputting sound to a non existent HDMI speakers.

    Yes it does beep for the initial group click - that doesn't annoy me because I'm accustomed to it.

    May be a workaround is to mute the speaker.

     

    It appears that most of you haven't read my Design Challenge posts which mention that to use EAGLE successfully you have to rewire your thinking to match the logic of its original designers.

    It's not dissimilar to German cars where you turn on a switch to turn on a light that which indicates that you've turned off the Air Conditioning.

    The designers appear to use the same core libraries for each all of the modules (PCB, Schematic and Library Manager) to make them very efficient which explains why some actions don't necessarily match the operator's assumptions and also have made the program platform agnostic (pc, mac, Linux).  It can be infuriating at first but once you've adapted and become accustomed it works very well.

     

    One big gotcha is that the default configuration EAGLE assumes that the user has a 3 button mouse - with the middle button used panning the current view.

    For one of my mice it's the scroll wheel button.

     

    Another gotcha for the Schematic Editor is to place Nets and not Lines. The Net tool differs from the normal Line tool by performing the extras required for net management.

    If you have used lines inadvertently they can bite you on your proverbials later on.