EAGLE User Support (English) EAGLE v8.0 Implicit Group   Command (Yeh) and Beeps on Every Left-Button Click (Boo)
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
  • Replies 11 replies
  • Subscribers 183 subscribers
  • Views 2438 views
  • Users 0 members are here
Related

EAGLE v8.0 Implicit Group   Command (Yeh) and Beeps on Every Left-Button Click (Boo)

autodeskguest
autodeskguest over 9 years ago

Trying to keep an open mind about v8.0 and hoping that the licensing issues

will work themselves out....

 

For for now, seeing what's different.  First thing I noticed is that EAGLE

finally has implicit grouping.  I suggested this years ago and finally it's

made it in.  Basically, if you don't have a command active and you draw a

rectangle it will create an EAGLE group as if you ran the EAGLE group

command (not persistent groups like other CAD software has, but essentially

a temporary group for the next command, like EAGLE has always had).

 

So that is great.  That will save lots of mouse clicks once I get used to

it.

 

But.....

 

Now I get an error beep on the first left-mouse button click whenever a

command isn't active, including the first corner of a group.  That is super

annoying.  For instance, in the schematic editor, a left-click anywhere

(with no command active) will beep AND start creating the first line in a

polygon for creating a group.  Very similar in PCB editor.

 

Also, when I run the group command I get a beep on the first mouse click

even when EAGLE should know that clicking in an area with no objects is

actually expected.

 

I assume that this is maybe something that somehow got missed (maybe the

sound was down) when implementing the implicit group function.  But it

should be fixed as it is really annoying.

 

Cheers,

 

James.

--

James Morrison  ~~~  Stratford Digital

http://www.stratforddigital.ca

--

http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

 

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 9 years ago in reply to rachaelp +1
    That's sure some Wile E. Coyote. Beep, Beep! I don't get any beeping at all with 8.0.2. (Windows) What procedure are you performing. All I do is press ESC and that defaults to the Group tool , left drag…
  • COMPACT
    COMPACT over 9 years ago in reply to rachaelp +1
    Silly me! My PC was outputting sound to a non existent HDMI speakers. Yes it does beep for the initial group click - that doesn't annoy me because I'm accustomed to it. May be a workaround is to mute the…
  • rachaelp
    rachaelp over 9 years ago in reply to COMPACT

    COMPACT wrote:

     

    Silly me!

    My PC was outputting sound to a non existent HDMI speakers.

    Yes it does beep for the initial group click - that doesn't annoy me because I'm accustomed to it.

    May be a workaround is to mute the speaker.

    No need to mute the speaker, you can turn the beep off in the settings.

    COMPACT wrote:

     

    It appears that most of you haven't read my Design Challenge posts which mention that to use EAGLE successfully you have to rewire your thinking to match the logic of its original designers.

    It's not dissimilar to German cars where you turn on a switch to turn on a light that which indicates that you've turned off the Air Conditioning.

    The designers appear to use the same core libraries for each all of the modules (PCB, Schematic and Library Manager) to make them very efficient which explains why some actions don't necessarily match the operator's assumptions and also have made the program platform agnostic (pc, mac, Linux). It can be infuriating at first but once you've adapted and become accustomed it works very well.

    Agreed. I think as soon as you understand that the UI is simply a front end for the command line commands then reading and understanding how they work makes it all fall into place. It did for me anyway.

    COMPACT wrote:

     

    One big gotcha is that the default configuration EAGLE assumes that the user has a 3 button mouse - with the middle button used panning the current view.

    For one of my mice it's the scroll wheel button.

     

    Another gotcha for the Schematic Editor is to place Nets and not Lines. The Net tool differs from the normal Line tool by performing the extras required for net management.

    If you have used lines inadvertently they can bite you on your proverbials later on.

    Useful tips for people new to EAGLE. On the subject of the mouse, before v8 it was a little awkward on a Mac to change routing layer as the mac doesn't have a middle button! This has at least been fixed in v8 :-)

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<