Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Revert net name back to default
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 187 subscribers
  • Views 2225 views
  • Users 0 members are here
Related

Revert net name back to default

autodeskguest
autodeskguest over 9 years ago

Hi,

I'm using EAGLE v6.6 on Windows 7 64-bit.

 

Is there a way to tell EAGLE to generate again a random name for a net

previously named?

 

I mean:

 

1. say you have a net called N$4

2. using the NAME command you change it to FOO

3. now I want to revert back to a default name, like N$*

 

I looked in the docs about NET command and NAME pages without find an

answer.

 

Marco

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    On 2/16/2017 3:02 AM, Marco Trapanese wrote:

    Hi,

    I'm using EAGLE v6.6 on Windows 7 64-bit.

     

    Is there a way to tell EAGLE to generate again a random name for a net

    previously named?

     

    I mean:

     

    1. say you have a net called N$4

    2. using the NAME command you change it to FOO

    3. now I want to revert back to a default name, like N$*

     

    I looked in the docs about NET command and NAME pages without find an

    answer.

     

    Marco

     

    Hello Marco,

     

    I hope you're having a good day. That's an unusual use case, thanks for

    bringing it up.

     

    If there are multiple nets named FOO in your design, then they are all

    interconnected.

     

    The easiest and safest thing to do is to delete the net and just redraw

    it, EAGLE will assign it an N$ name.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    --

    We have a new forum here <http://forums.autodesk.com>

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Il 16/02/2017 19:58, Jorge Garcia ha scritto:

     

    I hope you're having a good day. That's an unusual use case, thanks for

    bringing it up.

     

     

    To me, it happens when I have to insert a component in the middle of an

    existing net. I delete one segment, place the new component and

    reconnect both sides (I'm talking of two pins components, like R, C, L,

    D....).

     

    If I had previously named the net, it keep its own name, at least at one

    side. If I need to have the other side to the given name, I need to

    revert back to an "un-meaningful" name the first and set again the

    desired name to the second.

     

     

    If there are multiple nets named FOO in your design, then they are all

    interconnected.

     

     

    For my (personal?) use case, it should apply only to that segment.

    Because is there I broke the net to place a new component.

     

    I'll try the ulp of warrenbrayshaw and see if it fits!

    Thanks

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 9 years ago in reply to autodeskguest

    Hi,

     

    aha, ok, that's easy i think.

    After that if you merges two segments together to one segment, the menu

    will ask you, e.g.: "you are connecting two segments;;; the result name will: "...this name, or this name..";; is this ok?"" or similar.

    Well, that is easy for N$xx wires. -> just connect it and the suggested name N$xx appears.

    This will normally the latest wire number, or the first unused N$xx; e.g. N$1 ( or if N$1 is used, N$2 will come).

     

    Other think about is if you have power wires. Here you have priority usage of this wires.

    E.g.

    VSS -> GND => GND; GND -> VSS => VSS;

    // because you have supply pins on mostly components, you needs to check it manually.

    image

    Here in this example: AGND (analogGND) or VSS; but GND (some other have VSS as GND) are power pins of the ICs.

    What i want to say: "The wire with that you're going, this wire likes merging to the other and this (other) will you get, or what you want, ... normally."

     

    Best Regards,

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 9 years ago in reply to autodeskguest

    Hi,

     

    aha, ok, that's easy i think.

    After that if you merges two segments together to one segment, the menu

    will ask you, e.g.: "you are connecting two segments;;; the result name will: "...this name, or this name..";; is this ok?"" or similar.

    Well, that is easy for N$xx wires. -> just connect it and the suggested name N$xx appears.

    This will normally the latest wire number, or the first unused N$xx; e.g. N$1 ( or if N$1 is used, N$2 will come).

     

    Other think about is if you have power wires. Here you have priority usage of this wires.

    E.g.

    VSS -> GND => GND; GND -> VSS => VSS;

    // because you have supply pins on mostly components, you needs to check it manually.

    image

    Here in this example: AGND (analogGND) or VSS; but GND (some other have VSS as GND) are power pins of the ICs.

    What i want to say: "The wire with that you're going, this wire likes merging to the other and this (other) will you get, or what you want, ... normally."

     

    Best Regards,

    Gerald

    ---