Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Placing vias off grid
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 187 subscribers
  • Views 652 views
  • Users 0 members are here
Related

Placing vias off grid

autodeskguest
autodeskguest over 9 years ago

Hi,

quite often it happens to place components off grid. The common case is

when you have several IC with different pin pitches.

 

One issue I have is to place vias on tracks off grid.

Simple example:

 

1. place a component with pins off grid

2. route tracks (say horizontally) from those pins straight out (i.e.

you will have parallel tracks spaced by the IC pitch)

3. now you want to connect a wire (vertically) to one of the tracks,

using a via

 

Best case: the vertical track is on grid. So only the Y position of the

via is off grid.

 

Worst case: also the vertical track is off grid. Both X and Y

coordinates of the via will be off grid.

 

 

The only way I found is:

 

1. start routing from the off grid track (in the worst case it doesn't

matter which of course), in this example I assume the horizontal one

2. set the wire bend settings to the right corner

3. change layer so the via is placed automatically

4. connect to the other track

5. with the info tool copy the X coordinate of the vertical track

6. close the info tool, and open it again on the via

7. past the value to the X coordinate

 

Now you have the via properly aligned with the vertical track.

It takes a long time if you have to route dozens of tracks!

 

And if both tracks are off grid you have to repeat the process twice, or

at least you have to move around them to go on grid.

 

 

I never wrote an ulp so before start learning I would ask if it is

possible to do the following.

 

I'm thinking about an alignment aid. The flow would be this:

 

1. route the new track regardless the grid

2. right click on each end and select "align to"

3. specify the reference (if it's a track the correct axis is inferred

automatically - the one that doesn't change, it it's an object or a via

it could ask for X or Y)

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    On 26/02/2017 3:10 a.m., Marco Trapanese wrote:

    Hi,

    quite often it happens to place components off grid. The common case is

    when you have several IC with different pin pitches.

     

    One issue I have is to place vias on tracks off grid.

    Simple example:

     

    1. place a component with pins off grid

    2. route tracks (say horizontally) from those pins straight out (i.e.

    you will have parallel tracks spaced by the IC pitch)

    3. now you want to connect a wire (vertically) to one of the tracks,

    using a via

     

    Best case: the vertical track is on grid. So only the Y position of the

    via is off grid.

     

    Worst case: also the vertical track is off grid. Both X and Y

    coordinates of the via will be off grid.

     

     

    The only way I found is:

     

    1. start routing from the off grid track (in the worst case it doesn't

    matter which of course), in this example I assume the horizontal one

    2. set the wire bend settings to the right corner

    3. change layer so the via is placed automatically

    4. connect to the other track

    5. with the info tool copy the X coordinate of the vertical track

    6. close the info tool, and open it again on the via

    7. past the value to the X coordinate

     

    Now you have the via properly aligned with the vertical track................

     

     

     

    Most people use the freehand approach to this challenge, eyeballing it

    into place.

     

    Set the alternate grid to finest. Then with the ALT key depressed, move

    the via with its attached routing segments to where you need them.

     

    HTH

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

    ... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

    support forums.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Il 26/02/2017 03:34, warrenbrayshaw ha scritto:

     

    Most people use the freehand approach to this challenge, eyeballing it

    into place.

     

    Set the alternate grid to finest. Then with the ALT key depressed, move

    the via with its attached routing segments to where you need them.

     

     

    It could work, but it's not so easy to put a via at the exact

    coordinates by eye. I know myself: I will inspect the position to be sure image

    On the other hand EAGLE is a CAD! Hence I would expect some facilities

    to position and align objects.

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Il 26/02/2017 03:34, warrenbrayshaw ha scritto:

     

    Most people use the freehand approach to this challenge, eyeballing it

    into place.

     

    Set the alternate grid to finest. Then with the ALT key depressed, move

    the via with its attached routing segments to where you need them.

     

     

    It could work, but it's not so easy to put a via at the exact

    coordinates by eye. I know myself: I will inspect the position to be sure image

    On the other hand EAGLE is a CAD! Hence I would expect some facilities

    to position and align objects.