EAGLE User Support (English) grounded hole?
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 2025 views
  • Users 0 members are here
Related

grounded hole?

autodeskguest
autodeskguest over 10 years ago

Normally, I want my mounting holes isolated from the circuit. However, in a

board I'm working on, I want one hole to connect to the ground plane

(polygon). I made a large via with the drill size the same as the mounting

hole drills. And I put a large circle of tStop around the via for the screw

head. Is this the correct way to do this?

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 09/11/15 18:12, David Pollum wrote:

    Normally, I want my mounting holes isolated from the circuit. However, in a

    board I'm working on, I want one hole to connect to the ground plane

    (polygon). I made a large via with the drill size the same as the mounting

    hole drills. And I put a large circle of tStop around the via for the screw

    head. Is this the correct way to do this?

     

    It doesn't sound wrong, per-se, but have you looked at the "mount pad"

    devices in the "holes" library that comes with Eagle?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Rob Pearce wrote on Mon, 09 November 2015 13:21

    It doesn't sound wrong, per-se, but have you looked at the "mount pad"

    devices in the "holes" library that comes with Eagle?

     

    Rob - I forgot all about those. Thanks.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    You can create a grounded mounting hole as a DEVICE in your EAGLE library.  Use a pad with desired drill and diameter in the PACKAGE section, and then create a ground (or chassis) symbol for it in the SYMBOL section.  Connect pad and pin together and give it a name like "GP", for example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    You can create a grounded mounting hole as a DEVICE in your EAGLE library.  Use a pad with desired drill and diameter in the PACKAGE section, and then create a ground (or chassis) symbol for it in the SYMBOL section.  Connect pad and pin together and give it a name like "GP", for example.