Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Peltier Cooling Module Data sheet understanding
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 186 subscribers
  • Views 2906 views
  • Users 0 members are here
Related

Peltier Cooling Module Data sheet understanding

autodeskguest
autodeskguest over 10 years ago

I am working on a project which envolves the implementation of Peltier

modules. I am a mechanical engineering student. Currently, I am dealing

with a Peltier cooling Module whose data sheet is shown below in the

link from Farnell UK. We have Peltier cooling modules in the project

which are supposed to cool down some flowing air. This is the first time

I encounter Peltier modules.

http://www.farnell.com/datasheets/1693164.pdf

(https://mail.yandex.com/re.jsx?h=a,ggFabqW2FW_fTrpozMU2CQ&l=aHR0cDovL3d3dy5mYXJuZWxsLmNvbS9kYXRhc2hlZXRzLzE2OTMxNjQucGRm)

 

1-

I would like to ask about any good books available on the

Thermo-electric effect, and more particularly Peltier modules, the

physics behind them, mathematical models of them and their

implementation.

 

2-

Also I would like to ask about the performance graph of the Peltier

module (see the link below). According to what I understood from the

explanation available on the Internet, the Pc notation on the graph

refers to the cooling power. Is it the rate at which heat energy is

absorbed on the cold side ??

 

3-

There is a heat little heat exchanger which consists of a heat sink,

which holes filled in it and pipes are connected to flow water through

the heat sink to increase the convective heat loss and prevent any

overheat. While Tc the temperature on the cold side, can Th be

considered as the ambient temperature ?

 

http://oi57.tinypic.com/34hj2m8.jpg

(https://mail.yandex.com/re.jsx?h=a,Ve6XfGxq9DeW05E65tYxrQ&l=aHR0cDovL29pNTcudGlueXBpYy5jb20vMzRoajJtOC5qcGc)

 

4-

On the performance graph, the "Th" at which the data in the graphs were

collected is noted to be 25 C. Does this mean that I can refer to the

graphs only in case that that the temperature on the hot side at that

temperature ??

 

This because I found some sources on the Internet claiming at an offset

of ±10 C, with a slight margin of error.

 

 

5-

The other thing I need to understand is that if my understanding of the

cooling power "Pc", and if the temperature on the hot side "Th" remains

constant as shown on the graph, for a given value of current as shown

with the ascending lines on the right side in the lower section of the

graph, why would the cooling power (the power absrobed on the cold side)

fall if the temperature on the cold side falls as well. If my

understanding of the cooling power is correct, then wouldn't the

temperature of the cold side drop as more power "Pc" is absrobed ??

 

 

6-

In the lower section of the graph, if I choose two different

intersection points on the straight line of the current value 4.8 Amp,

when at "Tc = -20 C & Pc = 40 W" and when at "Tc = -5 C & Pc = 60 W",

the corresponding temperature differential "dT" between "Tc" and "Th" is

"45 C" and "30 C" in relation to the "Th" shown on the graph

respectively. Thus, on the upper section of the graph, on the current

line of 4.8 Amp, the intersection of the line with "dT= 45 C" & "dT= 30

C", yields voltage values of "V= 24.5 volts" & "V=23.5 volts"

respectively. How can the same amount of current, and slight difference

in voltage create a substantial difference in the temperature on the

cold side ??

 

 

7-

How can I start with the implementation of the Peltier module, as I need

a starting point. According to what I understood, I need to specify the

temperatures I need on both sides of the module, with the cooling power

(the power to be absorbed on the cold side, if my understanding of the

cooling power shown on the graph is correct), so that I can specify the

electric current value I need. Based on the temperature differetial

between the hot and the cold side, and the value of the current, I can

then determine the value of voltage I need to supply to the Peltier

module, so that it generates the difference in temperature I need. Am I

on the right track, and is there any piece of advise that I can make use

of ??

 

 

Sorry for the very long thread.

 

Thanks in Advance

 

Regards

 

--

To view any images and attachments in this post, visit:

http://www.element14.com/community/message/163918

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    Hi Banshee,

    I will ask  to move your question to a better group.

    John

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/166186

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago

    Hi Banshee,

    I will ask  to move your question to a better group.

    John

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/166186