Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) BUG: enter doesn't work in control panel
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 187 subscribers
  • Views 754 views
  • Users 0 members are here
Related

BUG: enter doesn't work in control panel

autodeskguest
autodeskguest over 10 years ago

I just installed version 7.5.0, and ran into a new bug.  I can navigate

thru the file tree view in the control panel as usual, but ENTER doesn't

work anymore to cause a file to be opened.  Apparently you have to double

click.

 

This is a rather blatant bug to slip thru.  It shows that your developers

use the mouse instead of the keyboard.  That's a preference, but everything

still needs to be checked using the keyboard as much as possible.

 

Personally, I prefer to type rather than click, because typing is so much

faster.  One of the great things about Eagle is that the underlying system

is command based, so that you can enter commands with the keyboard.

Between that and the flexible hot key system, you can really navigate and

control Eagle quickly with the keyboard.  The mouse only needs to be used

for inherently graphical interactions.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • geralds
    geralds over 10 years ago

    Hi,
    i also work with the 7.5.0 on windows 10 pro.


    In the panel you can also opening or closing the folders with the space button.
    And also with the space button you can opening the project files; e.g. sch and pcb.

    Yes the enter button doesn't work. This seems a bug.

     

    Of the other hand I think this would be good because the enter button is a little bit strong command, isn't it?

     

    regards

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 10 years ago

    Hi,
    i also work with the 7.5.0 on windows 10 pro.


    In the panel you can also opening or closing the folders with the space button.
    And also with the space button you can opening the project files; e.g. sch and pcb.

    Yes the enter button doesn't work. This seems a bug.

     

    Of the other hand I think this would be good because the enter button is a little bit strong command, isn't it?

     

    regards

    Gerald

    ---