Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Plated Through Slots
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 1059 views
  • Users 0 members are here
Related

Plated Through Slots

dukepro
dukepro over 8 years ago

 

Good afternoon, all,

 

What is the best way to designate a slot to be plated through?

Essentially, I need an oval shaped hole that's plated through.

 

Eagle v7.7.0.

 

Ideas?

 

Thanks,

    - Chuck

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 8 years ago

    On 18.04.2018 22:38, Chuck Huber wrote:

     

    Good afternoon, all,

     

    What is the best way to designate a slot to be plated through?

    Essentially, I need an oval shaped hole that's plated through.

     

    Eagle v7.7.0.

     

    Ideas?

     

    Thanks,

        - Chuck

     

     

     

    Ive done this quite a few times (Eagle 7.7.0). It works best on library

    parts because then you can control each layer in the same go. Adding a

    milled slot directly on the board requires careful planned routing

    around and under it.

     

    In the package editor, I start with a pad somewhere at one corner/end of

    the slot. If you set the pad hole size to the mill width, you can get a

    better impression how much copper you need around the slot. Then I add

    the mill shape over the pin. In some cases a oblong pad may be the

    correct shape, but if not, I draw a polygon on each of the 16 layers,

    even if Im only using just a few of them. Make sure the polygons

    generates a "rest edge" as large as the rest-ring of the pad. Always add

    stop and paste layers to polygon pads. You may disalbe the pad's stop

    and paste, but they should ideally merge with the one you draw.

     

    Remember to send the gerbers of the mill layer and write a doc how to

    use it.

     

    The manufacturer will most likely understand that milled patterns in the

    middle of all-layers copper island should be plated, but you better add

    it to the docs too.

     

    Note:If you embed the slots in polygons, the fill thermals maybe have

    some connection issues with polygon pads. Make sure they look ok, or

    disable thermals of the polygons. Also note the added heat required to

    solder these slots.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 8 years ago in reply to autodeskguest

    On 04/19/2018 07:42 AM, Morten Leikvoll wrote:

    On 18.04.2018 22:38, Chuck Huber wrote:

     

    Good afternoon, all,

     

    What is the best way to designate a slot to be plated through?

    Essentially, I need an oval shaped hole that's plated through.

     

    Eagle v7.7.0.

     

    Ideas?

     

    Thanks,

         - Chuck

     

     

     

    Ive done this quite a few times (Eagle 7.7.0). It works best on

    library parts because then you can control each layer in the same go.

    Adding a milled slot directly on the board requires careful planned

    routing around and under it.

     

    In the package editor, I start with a pad somewhere at one corner/end

    of the slot. If you set the pad hole size to the mill width, you can

    get a better impression how much copper you need around the slot. Then

    I add the mill shape over the pin. In some cases a oblong pad may be

    the correct shape, but if not, I draw a polygon on each of the 16

    layers, even if Im only using just a few of them. Make sure the

    polygons generates a "rest edge" as large as the rest-ring of the pad.

    Always add stop and paste layers to polygon pads. You may disalbe the

    pad's stop and paste, but they should ideally merge with the one you

    draw.

     

    Remember to send the gerbers of the mill layer and write a doc how to

    use it.

     

    The manufacturer will most likely understand that milled patterns in

    the middle of all-layers copper island should be plated, but you

    better add it to the docs too.

     

    Note:If you embed the slots in polygons, the fill thermals maybe have

    some connection issues with polygon pads. Make sure they look ok, or

    disable thermals of the polygons. Also note the added heat required to

    solder these slots.

     

    Good morning, Morton and Paul,

     

    That's about what I was thinking as well.  I hadn't thought about

    putting a manual rest ring in on all layers, nor the mask.  The pad

    confirming the finished hole size is another good idea.  All good ideas.

     

    I agree with the problems of using the milling layer on the board.  It's

    very easy to overlook a trace crossing over it - I've don't it.  As

    such, I use the dimension layer for non-plated slots to allow the DRC to

    catch such errors.

     

    The copper around the slot and a note in the README should queue the

    board house to route the slot prior to plating, or at least to call me

    if they're left scratching their heads.

     

    Thanks,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 8 years ago in reply to autodeskguest

    On 04/19/2018 07:42 AM, Morten Leikvoll wrote:

    On 18.04.2018 22:38, Chuck Huber wrote:

     

    Good afternoon, all,

     

    What is the best way to designate a slot to be plated through?

    Essentially, I need an oval shaped hole that's plated through.

     

    Eagle v7.7.0.

     

    Ideas?

     

    Thanks,

         - Chuck

     

     

     

    Ive done this quite a few times (Eagle 7.7.0). It works best on

    library parts because then you can control each layer in the same go.

    Adding a milled slot directly on the board requires careful planned

    routing around and under it.

     

    In the package editor, I start with a pad somewhere at one corner/end

    of the slot. If you set the pad hole size to the mill width, you can

    get a better impression how much copper you need around the slot. Then

    I add the mill shape over the pin. In some cases a oblong pad may be

    the correct shape, but if not, I draw a polygon on each of the 16

    layers, even if Im only using just a few of them. Make sure the

    polygons generates a "rest edge" as large as the rest-ring of the pad.

    Always add stop and paste layers to polygon pads. You may disalbe the

    pad's stop and paste, but they should ideally merge with the one you

    draw.

     

    Remember to send the gerbers of the mill layer and write a doc how to

    use it.

     

    The manufacturer will most likely understand that milled patterns in

    the middle of all-layers copper island should be plated, but you

    better add it to the docs too.

     

    Note:If you embed the slots in polygons, the fill thermals maybe have

    some connection issues with polygon pads. Make sure they look ok, or

    disable thermals of the polygons. Also note the added heat required to

    solder these slots.

     

    Good morning, Morton and Paul,

     

    That's about what I was thinking as well.  I hadn't thought about

    putting a manual rest ring in on all layers, nor the mask.  The pad

    confirming the finished hole size is another good idea.  All good ideas.

     

    I agree with the problems of using the milling layer on the board.  It's

    very easy to overlook a trace crossing over it - I've don't it.  As

    such, I use the dimension layer for non-plated slots to allow the DRC to

    catch such errors.

     

    The copper around the slot and a note in the README should queue the

    board house to route the slot prior to plating, or at least to call me

    if they're left scratching their heads.

     

    Thanks,

        - Chuck