Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51066 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Richard,

     

    I recently sent a completed set of gerber files generated from Eagle to a PCB manufacturer. They replied saying that "no stackup information was provided in the gerber files." They needed further information on the thickness/material of the board and each of its layers. I have all of the layer specified in the DRC options for my board. My question is this: Does Eagle automatically generate the "stackup" information or do I need to manually create a text file and include this information for my PCB manufacturer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Joey,

     

    the layer setup is part of the Design Rules, which are stored in the board file. This means hat the board manufacturer can look up the setup if he would load the file in the layout editor and look into the Design Rules.

    There he can find the values for thickness and the via lenghts.
    But it is always good to tell the board house such details like setup and via lengths in a separate note. So I'ld recommend to tell them all details separately.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Joey,

     

    the layer setup is part of the Design Rules, which are stored in the board file. This means hat the board manufacturer can look up the setup if he would load the file in the layout editor and look into the Design Rules.

    There he can find the values for thickness and the via lenghts.
    But it is always good to tell the board house such details like setup and via lengths in a separate note. So I'ld recommend to tell them all details separately.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 14 years ago in reply to Dusan_R

    Hi Dusan,

     

    I will keep you message in mind and look into the Design Rules subject we discussed here as soon as I have a bit of time for this. Seems to be a bit odd....

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Dusan_R
    Dusan_R over 14 years ago in reply to Richard_H

    Yes, I might have done it. But everytime I reopen Eagle, the design rules

    are declared default, even though they are set correctly. Also in the XML

    data there is the header and description of the defaul rules instead of the

    rules I have in used indeed. Only after I load the rules from the file I

    have saved it looks OK - but only before the session is closed. A bit

    confusing...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to Dusan_R

    Hi Dusan,

     

    you never bothered me..... I am glad about each message that can help in improving EAGLE.
    I did some testing as well and could not find a problem with the Design Rules. So maybe you unintentionally changed the rules or loaded another dru file.

     

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Dusan_R
    Dusan_R over 14 years ago in reply to Richard_H

    Hi Richard,

     

    I have made more detailed look at it and I think you are right, the rules

    seems to be really saved, but if you open the DRC, in the headline the

    default rules are declared instead of the really used rules (I think in past

    there were the used rules with the indicator of change). I don't know why my

    rules were switched do default, perhaps I have unintentionally loaded it,

    but the false indication confused me...

    I am just finishing one thing I have begun in 6.x and continue only in 5.11

    (at least upto the next upgrade), so you will not be bothered from my side

    so much now...

     

    Regards  Dusan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Dusan_R
    Dusan_R over 14 years ago in reply to Richard_H

    Hi Richard,

     

    yes, it is what I would expect, but why if I close project and re-open it,

    the Design rules are switched to default? I was surprised by the number of

    errors and it is why I noticed this. Now I have to save rules in separate

    file and open them after each Eagle restart - perhaps something is wrong at

    my side, but I do eherything the same way I am used from past.

     

    Dusan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to Dusan_R

    Hi Dusan,

     

    the Design Rules are part of the board file. When i look into a version 6 board file I can see the Design Rules section. As you can see here.....


    ......

    ......

    <designrules>
    <description language="de">&lt;b&gt;EAGLE Design Rules&lt;/b&gt;
    &lt;p&gt;
    The default Design Rules have been set to cover a wide range of applications. Your particular design may have different requirements, so please make the necessary adjustments and save your customized design rules under a new name.</description>
    <param name="layerSetup" value="(1*2+3*16)"/>
    <param name="mtCopper" value="0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm 0.0356mm"/>
    <param name="mtIsolate" value="0.38mm 0.71mm 0.38mm 0.1499mm 0.2007mm 0.1499mm 0.2007mm 0.1499mm 0.2007mm 0.1499mm 0.2007mm 0.1499mm 0.2007mm 0.1499mm 0.2007mm"/>
    <param name="mdWireWire" value="8mil"/>
    <param name="mdWirePad" value="8mil"/>
    <param name="mdWireVia" value="8mil"/>
    <param name="mdPadPad" value="8mil"/>
    <param name="mdPadVia" value="8mil"/>

    ......

    ......

    ......

     

    All the values are in the file.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Dusan_R
    Dusan_R over 14 years ago in reply to Richard_H

    Hi Richard,

     

    I am affraid the Design Rules are NOT stored in brd file, at least my 6.1

    doesn't store it, which in my opinion is another from long list of bugs with

    potentially serious consequences...

     

     

    Dusan