Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 55547 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Dear Mr. Hammerl,

     

    Im just starting a new PCB design with Eagle.

     

    I want to know where I cant find the library for the MAX8677C, MAX1674EUA.MAX1674EUA..

     

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago

    Dear Mr. Hammerl,

     

    Im just starting a new PCB design with Eagle.

     

    I want to know where I cant find the library for the MAX8677C, MAX1674EUA.MAX1674EUA..

     

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 16 years ago in reply to e14 Contributor

    There is good FAQ on the CadSoft website which covers also the subject

     

    Finding Libraries and Components

     

    I simply want to post it here as well. I hope this helps you in finding your components.

    <---begin--->

     

    In the Control Panel's tree view Libraries branch are listed all the libraries stored in the given library path(s) which is set by the menu Options/Directories. Most libraries provide a short description  of its content which is shown on the right half of the Control Panel as soon you click on one of the library entries in the tree view. Click the + character in front of the library name to unfold it, in order to see the Devices and  Packages in the library. Click on one of these entries and you will get a preview on the right.

    In addition there is a direct search function in the ADD dialog where you  select the components in order to place it in your schematic or layout. In the Schematic Editor it is possible to search for Devices.
    If you are looking for Packages, you have to do this in the  Layout Editor.
    Please note: The search function recognises only libraries that are in use (USE command). Whether a library file is in use or not can be checked quickly in  the Tree View's Libraries branch. If the marker behind the library name is green, it is in use. Is it grey, it's not in use and not taken into consideration by the search function.
    The ADD dialog has a Search line at the bottom. Enter the search pattern there. It makes sense to work with placeholders here. The asterisk * stands for any number of any character, while the question mark ? is used for exactly one single character. The options Smd and Description in the ADD dialog allow to extend the search for parts with smds and include the Device/Package descriptions.
    If you don't find an adequate part in one of the EAGLE default libraries take  a look at CadSoft's web server. In the Download area's Libraries directory are lots of user-contributed files available for free download. Otherwise it's  easily possible to define your own part in EAGLE.

    <---end--->

     

    By the way: The first place to look for would be maxim.lbr. At them oment i don't know if this component is available...try it.

    The second place to look for is on our web server, Download area, Library directory. There are lots of user-contributed libraries avilable.

     

    Hope this helps.

    Richard Hammerl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • KennyMillar
    KennyMillar over 16 years ago in reply to e14 Contributor

    Hope you don't mind me jumping in with a reply here...

     

    Well, as you'll have seen, Eagle ships with a huge library of parts, however it doesn't cover everything.

     

    You can also design your own libraries, and you can copy packages, devices and sumbols from one library to another.

     

    Many users also like to contribute their own libraries to the Eagle community, and you can find many of these if you go to www.cadsoftusa.com then click on downloads, and then libraries.

     

    If the exact device you need is not in one of the shipped libraries, or one of the user libraries, then spend a moment using google to see if anyone else has drawn your parts and made the library available, if that fails then you can draw it yourself in the library editor.

     

    Don't go re-inventing the wheel - copy a package and possibly a symbol from an existing library and add it to a new library of your own, then edit it to suit.

     

    As a general rule, don't add new devices to the shipped libraries as you may loose your changes at the next upgrade if you overwrite the editied library.

     

    Finally, if you do deisgn your own library and verify that it is correct, please consider uploading it to the cadsoft website so others can use it too!

     

    I hope you find this information useful.