Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51306 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • levafreidin
    levafreidin over 15 years ago in reply to e14 Contributor

       I think, by default "EAGLE" assume large copper ring around holes in pads and vias.

    Setting to check (I use EAGLE 4.16r2, hopefully difference is not dramatical) :

       Command   "DRC",  open "Restling", set both "Min" and "Max" equal 7 mils (<=0.2mm) for "Pads" and "Vias", set "%"  = 0.  "Apply".

    If it works, set values more siutable for your PCB.

           Best regards,

                Lev.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Nicole,

         I'm using EAGLE 5.11 and starting to submit my gerber filess to Sierra Circuits. Their Better DFM program flagged several issues all they say are due to "...oval shaped features are provided in "Line" mode whereas it should be in "Pad" mode...".

         Their DFM comment is "Plated holes that do not have a pad will not have an annular ring. There is a missing plated hole at ...", and 28 X,Y coordinates are given.

         Most of these occur on pins 1 through 8 of three occurences of part number Dil16.pac in resistor-dil.lbr. I looked  at this part and can tell no difference between pins 1-8 and pins 9-16!

         I used Excellon.cam and Gerb274x.cam to produce the files for this 2-Layer board.

    Any help is appreciated,

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Richard,

     

    How can I find the paths to the libraries that show up in the info dialog box? I need to modify a package per my manufaturer's request. But, I have from many different upgrades over the years librairies from different versions. My info box shows rcl-2 but there are four of them on my drive.

     

    thanks in advance

     

    steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago
    Dear Richard,
    I am using a professional EAGLE 5.11.0.
    I have created a component made of 100 connections.
    The package is a series of 4 alignments of pads drilled at 0.66mm and spaced of 1.27mm pitch.
    In the library package editor, while using a grid resolution of 0.01mm, we can see that the distance free of copper in between two pads is 0.22mm which is perfect regarding the PCB manufacturing precision.
    We are very surprised to see on the board layout generated from the schematic using this component that the actual distance free of copper in between two pads has dramatically reduced to 0.11mm which is far too tight.
    We have discovered this discrepancy with the DRC.
    Can you please explain how to correct this issue, may be a setting somewhere?
    Best regards,
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Hummingbird
    Hummingbird over 15 years ago

    Hi Richard

     

    Just tried to copy a part to our eagle library - got an error 5.9.0-1986 and now all the packages are gone from our library file.  We can see the symbols, bit no packages - any ideas?

     

    Norman

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    When doing the printjob, always a wrong time is shown on the grahics. It is not related to GMT al all.

    Example the graphics shows 13:23:33 the PC real time clock is 11:48.

    How can I synchronize it to a correct display. Eagle version 5.11.0 is in use.

    Thanks for the support.

     

    Horst

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • levafreidin
    levafreidin over 15 years ago in reply to e14 Contributor

    Helli John,

         In my libraries, I have few different "packages" for prototyping, like this:

     

    image

     

    This one accepts SOT23, narrow and wide SOIC, 0.3" and 0.6" DIP.

    For 0402 - 0805 discretes I use rectangular vias 76/42 mils,

    which I place on board after "GRID 0.1" command.

         Regards,

              Lev.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    A customer wished the unused area on the PCB to have pads on 0.1" centers for installing simple custom circuitry to handle changes that come up as boards are used in jet engine combustor testing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi John,

     

    yes I think so. Use vias and place them in the fitting grid. You can NAME the vias if you would like to have them connected to certain signals.

    As an alternative you could define this area in the library as a package with pads. Might be interesting, if you are working in the layout without consitent schematic in the background.


    What are you planning to do exactly?

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Richard,

     

         Are VIAs the best way to make small breadboard areas on a PCB?

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>