Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51426 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    hmm hi again,

    Ima trying to run CAM Job from batch file (resp. cmd) but dont have luck. For example I have singlesided.brd and i wann generate pokus.gbr with device as gerber_rs274x and layer pad via top... I write somethink like this:

    start "C:\Program Files\EAGLE-5.11.0\bin\eaglecon"  -X -gerber_rs274x  -opokus.gbr singlesided.brd via pad top, where i do mistake anybody help :-( 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    I think this is going to show how green I am but I am in need of a generic part for a 3 x 3 x 0.55 mm 20-pin QFN package. I am not sure of how accurately I can make this part from scratch.  Never tried to make a part before. I contacted the manufacture of this chip and they sent me a "PADS-LIBRARY-PCB-DECAL" file. I am not sure of what software this file is from but it looks like an ASCII based part file? Anyway to convert this? Any tip or links to a generic part lib?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to Rigor69

    Hi,

     

    the designlink interface/ULP does not support  other vendors, but of course you can define your own attributes for a component and add further infomation. Let's say you use the ATTRIBUTE command and define an attribute named INFORMATION for the component you can add further details and don't have to use the value for it. With the help of one of the bom.ulps you can export this information into your bill of material. Take bom_with_attributes.ulp from the CadSoft download, for example.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Rigor69
    Rigor69 over 15 years ago

    Hi, I am new to using the designlink, and i absolutley love it.

    However i do have a question:

    If the part i use cannot be found on farnell, how can i add other vendor product code in an attribute? i dont want to use the value field as it is too small snd should contain only the value...

    Thanks...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    thx for help :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Richard,

    Yes. You are right. The administrator mode solved my problem. Thank you.

    Best regards,

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Richard,   I want to connect two pads together with a trace on both layer 1 and layer 16.   I connect them together on the schematic, which leads to a single airwire on the layout.  Once I have connected that airwire - how do I make the other connection?  I would rather not do it "manually" because I am connecting many pads together this way.   Its for a general purpose prototype board.  Thanks in advance for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Peter,

     

    Windows 7 has more restrictions and in my opinion obstacles in user rights management than the Windows systems before. I am pretty sure that something on your system concerning user rights has changed. What you could try is to start EAGLE in Administrator mode. Therefore do a right mouse click onto the EAGLE icon and select "Run in administrator mode" or something like this from the context menu. Does it work as expected now?

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Bruno,

     

    I don't see any problems here. All the ULPs should run in the new EAGLE version.

    There are some slight changes in the EAGLE Script language which might cause an error in executing a script.... What you could do is to try your ULPs with our Freeware first.

    But I don't see serious problems....

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Dan,

     

    it is possible to have the libraries for example on a publicly available server directory. So everybody has access to the libraries. But think about library management. It would be a problem if everybody has write access to them. So it could happen that two ore more people edit the same library.... The one who saves the library last will win..... the work of his colleagues will be overwritten and lost.

    So it would be good to have only one user who has write access to the lbr folder. He can manage libraries and add new components and so on......


    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>