Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51507 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to rifo

    Hi Rifo,

     

    You can use the SMD command in the commandline of the Package Editor:

     

    SMD 0.5 0.2  (0 0) ( 2 0) (4 0)........

     

    This places SMDs with a size of 0.5 by 0.2 at the location (0 0) (2 0) and so on.

     

    Reagrds,
    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi,

     

    please check  http://www.element-14.com/community/docs/DOC-24843/l/eaglecomparepdf

    or take a look at the CadSoft website: http://www.cadsoftusa.com/prices.htm

    In case you have access to the PF intranet you could also check the CadSoft section.

     

    Regards,
    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rifo
    rifo over 15 years ago

    Hello,

     

    I am wondering if it's possible to use the SMD command to place multiple pads at different locations in a single command. I have read the help document and there does not seem to be a way to do this. I would be happy if you can guide me about this.

     

    Thanks for your time

    Rifo

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    I am looking for an EAGLE Selector guide on Element14.  Can you point me to the right location?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago in reply to e14 Contributor

    Hi Joe,

     

    Run the export-project-lbr.ulp in the schematic editor. This ULP will create libraries based on your design files. In my personal experience it tends to work best when you let it create multiple libraries.

     

    hth,

     

    Jorge Garcia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Richard,

     

    I recently made a new part for a design I am working on and used it in a schematic and a PCB.

    Unfortunatly, the library file of the part was deleted.

    The part still exists in the design, both in the schematic and the layout.

    Is there any way I can extract the part from the design and make it back into a library part?

     

    Thanks,

    Joe A

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Marc,

     

    this question was asked recently, I believe in the same thread. But since there more than 700 entries this thread begins (since a long time) to become more and more unreadable...... image

    But here a possible solution for your request:

     

    The Procedure:
    --------------------------------------------------
    Sometimes circuit boards will have duplicate sections of schematic that you
    want to layout identically.  You could do this by laying out each section
    separately, but for large or complex layouts this would be very time
    consuming.  Eagle does not have a function that allows you to directly
    duplicate your layouts, so you have to use this workaround:

     

    1. Create the schematic for the section you want to duplicate.  You can have
    additional schematic done at that time too if you like.
    2. Create the layout for that section.  You can have additional layout done
    at that time if you like.
    3. Close the layout so that you only have the schematic open.
    4. Use the window selection tool to surround the section of schematic you
    want to duplicate in the layout.
    5. Use the scissors tool to copy the selection to the buffer.
    6. Use the dropdown EDIT: PASTE to finish the copy operation.
    7. Save the schematic and close it.
    8. Open the layout. Click OK to acknowledge the warning about the schematic
    and board not being consistent. Close the schematic that opened when you
    opened the layout so that you only have the layout open.
    9. Do the same window select, scissors, paste operation on the layout.  YOU
    MUST COPY EXACTLY THE SAME ITEMS AS YOU DID IN THE SCHEMATIC.  THIS INCLUDES
    COMPONENTS AND NETS.
    10. Save the layout and open the schematic.  You should have both the
    schematic and layout open at this point.
    11. In the layout, run ERC and you'll get a long list of nets that don't
    match.  Don't worry: you only have to fix each net once.  This is usually
    only 5 or 6 nets to fix the whole list.
    12. The original section of layout will have nets named GND.  The new
    section will have them named GND1.  The original section of the schematic
    will have the nets named GND.  The new section will also have them named
    GND.  The task here is to rename the net GND1 to GND in the layout.
    13. Type "show GND1" in the command line.  This will highlight GND1.
    14. Use the name tool (R2 Icon) to change the name GND1 to GND.  If
    prompted, the rename applies to all nets.
    15. If you run ERC again, you'll find that all of the GND/GND1 errors are
    gone.  Redo this renaming process a few more times for the remaining name1
    nets and you're done.

     

    Additional note: If you don't have any airwires for the net you're trying to
    rename then you'll have to create one using the line tool and the name tool:
    Create a line.  Rename that line using the R2 tool to the net name you need
    to rename (e.g. GND1).  This will connect the line to the pad that was
    previously un-airwired.  Now you can rename the airwire or line to the right
    name (e.g. GND) to fix that net.
    --------------------------------------------------

     

    This was initially posted in the eagle.support.eng forum....

     

    Regards,

    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    I would like to import a part of a schematic/layout from one project  to another one without losing the extensive tracking that has already  been done . I can cut and paste a piece of the schematic but then the  pcb element is just a pile of components.

    Regards

    Marc

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    I would like to import a part of a schematic/layout from one project to another one without losing the extensive tracking that has already been done . I can cut and paste a piece of the schematic but then the pcb element is just a pile of components.

    Regards

    Marc

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi Jamie,

     

    the numbers 2,54/0,8 want to tell you that die drill diameter is 0.8mm (~32mil) and the diameter of the pad

    is 2.54mm (100mil). If you want to use smaller diameters you could change one of the packages there or define a new one with a smaller drill diameter.

     

    Regards,

    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>