Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51519 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

     

    I think that you may have miss read what I am trying to achieve.  The pad is to connect a 22 gauge wire to the PCB.

     

    Cheers,

    Jamie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hi again,

     

    you could define the pad diameter for the resistors in the library first, save the library file and use Library/Update in the Layout/Editor. So the resistors will be updated with the packages with bigger pads.

     

    Regards,

    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    I am totaly new to PCB design. In the wirepad library, I see a THROUGH-HOLE pad identified as 2,54/0,8; what is the interpretation of these numbers?  I am trying to place a wire pad to connect a 22 gauge wire (diameter .635mm or 0.025").  I have in the past placed a 0.04" hole.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Hi Richard,

     

    Sorry not so much image Settings for this circuit, now I am working on, is in this picture

     

    http://img576.imageshack.us/i/drc.png/

     

    I didn't decide on this values by some calculations, just tried and decide on whether the result is what i am looking for. And for this values the IC pads are ok. However pads for resistors and capacitors are not big enough for me. Because of this i am looking for a way to make bigger only some pads (resistor and capacitor pads).

     

    Meanwhile, select option on the DRC main window, for what i can use it? It is not similiar to rooting select option.

     

    I hope I'm much clearer now image

     

    Thanks Ahmet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Hello Ahmet,

     

    the restring settings are valid for all pads in the layout. What are the settings you are using for your pads.

    The width of the copper ring around the drilling is calculated in dependence of the drill diameter. But you can use equal values for minimum and maximum value, so that the width of  copper ring is always the same.

     

    Maybe this helps?

    Regards

    Richard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi, i need help about DRC rules. I prepare my circuits by using some hobby electronic techniques. And I'm using ofcourse eagle to draw them. However, when I change the DRC rules, especially the RESTRING option it changes the dimensions of all the component pads. And these are not equally the same for all of them. For example, the IC pads becomes much bigger than a resistor pad. And this is my problem. Is there any way to change only ressitor and capacitor pads. I know i can put extra via pads from the main BOARD window.

     

    Thank you, regards. Ahmet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi,

    Here is a Short Video of using Drag & Drop to copy components between libraries.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Jorge_Garcia

    Thanks, actually i figured it out with some tinkering. I didn't realize that it mirrored about an axis on the end, but when i did i couldn't move and mirror in the same step at first. I finally tried right clicking on it and went into properties and set the position for the axis for after i mirrored it and clicked the mirror radio box. Thanks for your consideration.

    -Jared

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago in reply to e14 Contributor

    Hi Jared,

     

    Send the board to support@cadsoftusa.com, I'll take a look at it. As a preliminary question, is the board oriented in such way so that it's largest direction is from left to right? The EAGLE size limitation is strictly 4" x 3", if you make a 3" x 4" board EAGLE won't allow you to place components at the very top of the board.

     

    See if this is perhaps your situation.

     

    hth,

    Jorge Garcia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 15 years ago in reply to e14 Contributor

    Hi Mike,

     

    1) There are a few ways to do this, but I think the easiest way is to:

     

    A. Open the library you want to copy into

    B. In the Control Panel find the package(symbol or Device)  you wish to copy and right-click

    C. In the cursor menu, select copy to library and you're done.

     

    As an extra hint, you'll find that the majority of standard packages are included in the ref-packages.lbr, so whenever you need a specific package check that library first.

     

    2) Remember that in EAGLE all connections are defined by name. In order to make a split power plane, you're going to use the POLYGON command. The polygon command allows you generate copper fills on the board. Once you've drawn the two fills you can use the INFO command to set the polygon properties and the NAME command to identify which net the copper pour will belong too.

     

    hth,

    Jorge Garcia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>