Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51100 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Hi again Richard,

     

    I didn´t explain well.

    I´m using Eagle v6 and as you said i have got connected one pin to various pads in the device editor. Now in the board layout i want to have a cooper track which goes from one element to these pads. The easy way is joining the element to one pad (of the connector) using the route command and then to do the same with the rest of pads(its a connector and these pads are very close one to another). But to make it " more beautiful" i though to join the element to one pad using route command and then with the rect make a rectangle joinig the four pads.

     

    It doesn´t work.

     

    Do you understand me now?

     

    Regards,

     

    Xabi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Hi Xabi,

     

    you wrote:

    If I have  four small pads (which have the same signal) and they are  very close, can I join one of them with the corresponding signal and  then use the "rect" command to join them ?

    Are you working with EAGLE V6? If yes, you can connect one pin to two or more pads in the device editor. You could also use a POLYGON (no RECT) in order to draw a special pad shape or to combine two pads.

     

    Hope this helps.

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor
    In Eagle 6.1.0, is there a way to get a printed ERC (and later a DRC) report? Text, PDF, or HTML would be acceptable.

     

    Hi Jerry,

     

    no I am sorry, currently not possible. Maybe you can make a screen shot of the ERC/DRC window?

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor

    Helo Sylvain,

     

    you wrote:

    how to represent a slot that needs to be milled and platted inside, what layer, what line width etc..?

    If the board manufacturer has to mill oblong holes, you have to draw the milling contour of oblong holes in a separate layer. Usually this is layer 46, Milling.
    The milling contour for components that need oblong holes can be drawn with WIRE (and possibly ARC) with a very fine wire width near or even 0 in the Package Editor. Take a pad that has a drill diameter which lies inside the milling contour, or SMDs, for example in Top and Bottom layer, as basis for the oblong hole.
    In case of a multilayer board you should draw a WIRE in the used inner layers at the position of the oblong holes so that it covers the milling contour and leaves a kind of restring around the opening. Please inform your board manufacturer that they have to take care on the milling data drawn in this layer.

     

    what type of CAM job to use in order that gerber files show properly the slots to be milled?

    You have to add a further sectino to your CAM job that exports Gerber data for layer 46 Milling.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 14 years ago in reply to e14 Contributor
    There is still a problem if the associated .brd file is not available.  In that case Eagle pops up only the Control Panel and the Schematic  editor. Focus is on the Control Panel so the command does not execute  until you click on the Schematic Editor window. That is a bit of an edge  case for me which I can work around by having a .brd file.


    Yes, the command  edit  .sch  needs a board file. If there is no board this could make trouble as well. I will forward this matter to the development team, because it really seems to be a timing problem of opening the editor windows.....

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Richard,

     

    If I have  four small pads (which have the same signal) and they are very close, can I join one of them with the corresponding signal and then use the "rect" command to join them ?¿

    I´m worried about that because you cannot insert the name in the rect, so i don´t know if it will work.

     

    Regards,

     

    Xabi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Richard,

    In Eagle 6.1.0, is there a way to get a printed ERC (and later a DRC) report? Text, PDF, or HTML would be acceptable.

     

    Thanks,

    ...jerry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi,

    I have designed a board using ALLEGRO ACS750*CA-050 (Farnell: 1791390) component for which I found the device in the Allegro library.

    This component requires two slots PTH of 2x4mm.

    Eurocircuit is the present manufacturer for our boards.

    It seems that the interpretation of the files sent to the manufacturer does not show properly the slots shape.

    The boards arrived with pairs of holes intead of the slots.

    Question 1 : how to represent a slot that needs to be milled and platted inside, what layer, what line width etc..?

    Question 2 : what type of CAM job to use in order that gerber files show properly the slots to be milled?

    kind regards,

    Sylvain

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Richard_H

    Hi Richard,

    could you modify your command line, so that the schematic file is explicitely loaded before the printing starts?

     

    It looks like this then:

     

    eagle  -C "edit .sch; print 0.59 SHEETS ALL LANDSCAPE PAPER Letter FILE .pdf;" mydesign.sch

     

    That does the trick.

     

    There is still a problem if the associated .brd file is not available. In that case Eagle pops up only the Control Panel and the Schematic editor. Focus is on the Control Panel so the command does not execute until you click on the Schematic Editor window. That is a bit of an edge case for me which I can work around by having a .brd file.

     

    I haven't had a chance to try the scripting idea and I'll keep it in mind for the future.

     

    Thanks for your help,

    ...jerry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Dusan_R
    Dusan_R over 14 years ago in reply to Richard_H

    Hello Richard,

     

    i think that there is a genereal problem in 6.1 with placing parts - also if

    I copy elements using COPY it is quite difficult to place part correctly -

    it tends to snap to the neighbouring grid position (in all directions), so

    sometimes I have to undo and try again several times until I place element

    correctly. 

    Currently I am considering going back to 5.11, because I think 6.1 is still

    not mature, but because od data incompatibility it would mean loss of a lot

    of work - BTW, I think that it would be great to have the possibility to

    back-convert the data or to have the option to save binary too (also because

    of much smaller files).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>