Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to remove mask stop for via?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 596 views
  • Users 0 members are here
Related

How to remove mask stop for via?

huayuliang
huayuliang over 16 years ago

on my board,  a few via need coated , don't need mask stop.

 

how can I do, such as my via's drill is 0.5mm, and diameter is 1.27mm,how can I set in design rules?

 

I have read this http://www.cadsoft.de/faq.htm.en#06062601, but can you give me a clear demo to me?

 

sorry for my bad english ,I can't understand that anwwer in faq.

 

Best reguards!

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 16 years ago

    Hello,

     

    by default all vias are not coverd with stop laquer because the Limit value is set to 0 in the Design Rule's Mask tab. You write your vias have a drill diameter of 0.5mm. So set the Limit to 0.5mm and you will see that all vias are covered. The stopmask symbols in the layer t/bStop vanish.

    This is valid for all vias on the board.

    And now you can use the CHANGE STOP command in the layout directly for each via. This can be done with groups also

     

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 16 years ago

    Hello,

     

    by default all vias are not coverd with stop laquer because the Limit value is set to 0 in the Design Rule's Mask tab. You write your vias have a drill diameter of 0.5mm. So set the Limit to 0.5mm and you will see that all vias are covered. The stopmask symbols in the layer t/bStop vanish.

    This is valid for all vias on the board.

    And now you can use the CHANGE STOP command in the layout directly for each via. This can be done with groups also

     

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • huayuliang
    huayuliang over 16 years ago in reply to Richard_H

    image

     

    sorry for my carelessness, I made wrong unit....

     

    E of EALGE !!! It's too easy for user.

     

    Sincere regards!