Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Updated pinheader.lbr
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 3227 views
  • Users 0 members are here
  • pin
  • pins
  • pin_headers
  • pin_header
Related

Updated pinheader.lbr

e14 Contributor
e14 Contributor over 10 years ago

Hi

 

I required some single-row headers with octagonal pads for a project. Didn't find a suitable library so i modified eagles default pinhead.lbr library to include octagonal pads for all single-row headers. Also made some minor updates around naming to make it easier for future scripts to modify this package further.

 

Feel free to use and hopefully it can replace eagles default pinhead library since this contains everything from the original library + more.

 

// Rikard

 

Edit: See my post below for details on the latest update

 

Edit 2: Not sure how i missed this package before. http://www.cadsoftusa.com/downloads/file/pinhead-2.lbr this also contains SMD packages for the headers. Why isn't this a part of the default library which comes with eagle on installation instead of the current one?

Attachments:
pinhead_v2.zip
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Small update:

    I have also included lockable packages for pin header 1X02 to 1X20 (higher pin counts seemed unreasonable). Basically same as con-molex.lbr package 22-23-2xxx but i added this option here as well to keep everything in one place and to make it easier to change between different styles during design.

    Attachments:
    6204.pinhead_v2.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    Small update:

    I have also included lockable packages for pin header 1X02 to 1X20 (higher pin counts seemed unreasonable). Basically same as con-molex.lbr package 22-23-2xxx but i added this option here as well to keep everything in one place and to make it easier to change between different styles during design.

    Attachments:
    6204.pinhead_v2.zip