Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Eagle Mac OS 7.5.0 - Open multiple schematics
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 458 views
  • Users 0 members are here
Related

Eagle Mac OS 7.5.0 - Open multiple schematics

eryk_spinar
eryk_spinar over 10 years ago

Hello,

 

How can I open multiple schematic and board files in eagle on MAC OS?

 

Currently when I open one schematic for one project, and attempt to open another, the first one is being closed automatically so I cant compare them side by side.

 

I dont have this problem on Windows? Or am I doing something wrong?

 

Thank you

Eryk

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 10 years ago

    HI,

    you can open only one pair of schematic and board. And one library file and a "unlimited" number of text editor files within one EAGLE instance. As far as I know MAC OS does not allow two instances of one application at the same time by default.

     

    Searching in the web gave a solution for this (with Textedit.app as example):

     

    If you use open from the command line you can pass a parameter to start a new instance:

    open -n /Applications/TextEdit.app 

    Another way is to find the Unix executable in the app bundle and run it:

    /Applications/TextEdit.app/Contents/MacOS/TextEdit & 

     

    Hope this helps.

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 10 years ago

    HI,

    you can open only one pair of schematic and board. And one library file and a "unlimited" number of text editor files within one EAGLE instance. As far as I know MAC OS does not allow two instances of one application at the same time by default.

     

    Searching in the web gave a solution for this (with Textedit.app as example):

     

    If you use open from the command line you can pass a parameter to start a new instance:

    open -n /Applications/TextEdit.app 

    Another way is to find the Unix executable in the app bundle and run it:

    /Applications/TextEdit.app/Contents/MacOS/TextEdit & 

     

    Hope this helps.

    Regards,

    Richard