Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to use parameters %C, %F and %L when designating an external text editor
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 1039 views
  • Users 0 members are here
Related

How to use parameters %C, %F and %L when designating an external text editor

Michael
Michael over 15 years ago

Is there anybody knows how to use parameters %C, %F and %L when designating an external text editor in EAGLE's Option Menu? I just learned from Internet that %F means only if this parameter is added in the command line, like "C:\WINDOWS\system32\notepad.exe" "%F", the ULP or SCR file can be opened directly in notepad, otherwise a new empty notepad will pop up.

 

Is there any more suggestions for %F? and %C and %L? Could anybody here give me some examples for the usage of these parameters?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    The usage of these parameters depends on the editor you wish to use, but I'm afraid that you can't use %C and %L with notepad. I am using MultiEdit and my command line looks as follows:

    Mew32.exe "%F" /NOSPLASH /RW /L%L /C%C

     

    Another exapmle is for notepad++:

    notepad++ -n%L -c%C "%F"

     

    But whatever editor you use, you need to look up it's documentation for the supported command line switches. You'll see then if the editor is able to take you to a particular line and column.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Michael
    Michael over 15 years ago in reply to e14 Contributor

    Thanks, but it doesn't work because I am using notepad of Windows XP. The command line I tried is notepad -3%L -2%C "%F", do you know where the error is? or maybe notepad never supported %L and %C?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Michael
    Michael over 15 years ago in reply to e14 Contributor

    Thanks, but it doesn't work because I am using notepad of Windows XP. The command line I tried is notepad -3%L -2%C "%F", do you know where the error is? or maybe notepad never supported %L and %C?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Richard_H
    Richard_H over 15 years ago in reply to Michael

    Hi,

     

    as far as i remember a posing in one of the CadSoft Newsgroups, notepad is not first choice here. It does not support all these options.......... The community likes notepad++  image

     

    Regards,

    Richard