Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum BGA & microvia howto
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 659 views
  • Users 0 members are here
Related

BGA & microvia howto

e14 Contributor
e14 Contributor over 14 years ago

Hi Richard,

 

I use Eagle software V6.2.

It is the first time I route a BGA component and I have difficulties to use the "route-bga.ulp" tool.

I get more then 400 DRC errors ! 2 types of error are listed: "drill distance" on layer 20 and "overlap" on layer 1,15 and 16.

See attached files for more details

 

Thanks by advance for your help.

 

Fabrice.

Attachments:
myfiles.zip
  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 14 years ago

    Hi Fabrice,

     

    it is not easy to find out what the problems are without having the orignal brd file, but there are some suggestions I have:

    1. please check the layer setup. You used  (((1*2)*3)*(14*(15*16)))  which is no good choice.
    This way EAGLE can't use micro vioas because there are none defined. You defined only through hole vias.

    My suggestion is:   [3:(1+(2*3)+(14*15)+16):14]  The brackets [] define blind vias, which can be used for micro vias too.

     

    2. Change the value for Via-SMD for Same signals to 0. So no errors should be reported for vias on SMDs.

     

    Hope this helps.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 14 years ago

    Hi Fabrice,

     

    it is not easy to find out what the problems are without having the orignal brd file, but there are some suggestions I have:

    1. please check the layer setup. You used  (((1*2)*3)*(14*(15*16)))  which is no good choice.
    This way EAGLE can't use micro vioas because there are none defined. You defined only through hole vias.

    My suggestion is:   [3:(1+(2*3)+(14*15)+16):14]  The brackets [] define blind vias, which can be used for micro vias too.

     

    2. Change the value for Via-SMD for Same signals to 0. So no errors should be reported for vias on SMDs.

     

    Hope this helps.

     

    Regards,

    Richard