Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum eagle wiring schematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 949 views
  • Users 0 members are here
Related

eagle wiring schematic

av8or1
av8or1 over 13 years ago

Ok I am frustrated. Too many times in eagle I have tried to wire chip pin to whatever else but the friggin wire won't connect to the pin. I discovered the trick of manually entering the x-y coordinates and that sometimes works. So how the heck do you go about doing this reliably?

  • Sign in to reply
  • Cancel
Parents
  • RayA
    RayA over 13 years ago

    Hi,

    I thought that there was a way to force a wire to snap to the nearest object, like doing a Control/click, or something, but I can't find a reference to that right now.

    Two causes for this problem that I can think of are:

         1- If the "Snap Length" has somehow gotten set very small. That setting is in Options/Set/Misc/Snap Length. It is 0.020" by default.

         2- If a component was defined in mm but your grid is set to inch, then the component pin probably isn't lined up with the snap grid. You can get around this by defining the alternate grid in mm. Then when you do an Alt/click, it will snap to the pin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • RayA
    RayA over 13 years ago

    Hi,

    I thought that there was a way to force a wire to snap to the nearest object, like doing a Control/click, or something, but I can't find a reference to that right now.

    Two causes for this problem that I can think of are:

         1- If the "Snap Length" has somehow gotten set very small. That setting is in Options/Set/Misc/Snap Length. It is 0.020" by default.

         2- If a component was defined in mm but your grid is set to inch, then the component pin probably isn't lined up with the snap grid. You can get around this by defining the alternate grid in mm. Then when you do an Alt/click, it will snap to the pin.