Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum eagle wiring schematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 949 views
  • Users 0 members are here
Related

eagle wiring schematic

av8or1
av8or1 over 13 years ago

Ok I am frustrated. Too many times in eagle I have tried to wire chip pin to whatever else but the friggin wire won't connect to the pin. I discovered the trick of manually entering the x-y coordinates and that sometimes works. So how the heck do you go about doing this reliably?

  • Sign in to reply
  • Cancel
Parents
  • AnalogNotes
    AnalogNotes over 13 years ago

    I understand the frustration!  It took me a long time to sort some things out with Eagle, but now that I have, I really love it...

     

    How is your grid set up?  Is it .1 inch?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • av8or1
    av8or1 over 13 years ago in reply to AnalogNotes

    Grid is set to 0.1 in both schematics. Both the wire and pin have the identical y coordinates. They clearly overlap precisely even on small scale close up viewing. Set the snap option from 20 mil to 80 mil. Saved the Library

    Updated all libraries. Still cannot get the friggin wire to connect to pin 5 of the device. Pin 5 is set as out type. The middle of that pin is right on a grid line. So is the wire. Trying like heck to get it to work but it won't.  I can connect a wire to pin 6. Haven't tried 4 yet.  Maybe I'll do that next. If I still can't get it to work I'll post pics.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • av8or1
    av8or1 over 13 years ago in reply to AnalogNotes

    Grid is set to 0.1 in both schematics. Both the wire and pin have the identical y coordinates. They clearly overlap precisely even on small scale close up viewing. Set the snap option from 20 mil to 80 mil. Saved the Library

    Updated all libraries. Still cannot get the friggin wire to connect to pin 5 of the device. Pin 5 is set as out type. The middle of that pin is right on a grid line. So is the wire. Trying like heck to get it to work but it won't.  I can connect a wire to pin 6. Haven't tried 4 yet.  Maybe I'll do that next. If I still can't get it to work I'll post pics.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • av8or1
    av8or1 over 13 years ago in reply to av8or1

    Ok I figured it out. Pins 2 and 6 wouldn't wire connect. All others would.  Strange. So I disconnected everything in the device editor. Went to the symbol editor. Deleted pins 2 and 6. Recreated them. Back to the device editor. Reconnected everything. Saved. Updated all libraries. Back to board schematic. Connected wires to pins 2 and 6. Moved the device around a bit, then back to its original location where the wires were overlapping again. Boom! A junction symbol appears for those two pins. Move the device around a bit, can see that they're connected.

     

    Dunno what the problem was but I'm a way don't care either.  Well actually I do but I gotta move on.

     

    Thanks. Hope this helps someone else.