Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Good battery for rc car project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 412 views
  • Users 0 members are here
Related

Good battery for rc car project

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I am working on a raspberrypi based rover. I got video streaming working and for the motors (2 of them), I am using an L298N Dual H-Bridge motor controller board.

The controller works fine, however, for the motor power supply (going + to VCC and - to GND), I used the li-ion battery that came with the basic rc car I bought. The battery is blank, but the charger says it outputs 4.8V at 250mA, and takes 8 hours for a complete charge.

 

When I test the car out, it works, but moves very slowly, and often stops. Without the weight, the car moves very swifty. It weighs less than 250g.

 

The motor looks like:

http://www.globalsources.com/gsol/I/DC-motor/p/sm/1056803236.htm

 

Can anyone suggest a good battery for the project, or atleast weather I need to up my mA or my voltage?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    Can you post a picture of the whole thing, car + load etc.

    If I understand you correctly the car is fine until you add some mechanical load and then it won't go very well - this might be  one of many problems and you need to provide more information to work out what's wrong.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 12 years ago

    Can you post a picture of the whole thing, car + load etc.

    If I understand you correctly the car is fine until you add some mechanical load and then it won't go very well - this might be  one of many problems and you need to provide more information to work out what's wrong.

     

    MK