Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum PCB based rogowski coil design software
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 189 subscribers
  • Views 4542 views
  • Users 0 members are here
  • rogowski
  • pcb
  • Design
Related

PCB based rogowski coil design software

e14 Contributor
e14 Contributor over 11 years ago

Hi guys,

I need to design a rogowski coil on a 2 layer PCB.

How can I draw a simply rogowski coil on a PCB software? Are there any ways i can do it?

It should look something like this:

image

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    With regards to using EAGLE to develop Rogowski coils, I got assistance from jorge <jorge.garcia@cadsoftusa.com> and he shared that:

    EAGLE unfortunately doesn't have any built-in mechanism to create rogowski coil structures. The only way to do it in EAGLE is to code in ULP to perform the mechanical calculations based on some input parameters and then script out the creation of these features.

    Hence i decided to try other software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    https://en.wikipedia.org/wiki/Rogowski_coil

    What are your plans or this?

    This will probable not work because: http://www.embedded.com/print/4010002

    Clem

    P.S. Forum for Electronics more information

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I tried using another software - CST Microwave and was successful in creating the desired design but have problems exporting it to gerber.

    Would appreciate if there's any other suggestions on designing and fabricating a PCB based rogowski coil.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    i managed to get Eagle working but unable to replicate the pattern in my first post (Rogoswki coil).

    Any tips I can achieve it? - the bottom trace should be connected to top trace at the Via.

    Picture below shows what i have managed to draw.

    image

     

    Also is it possible to automate the duplication process (PASTE command that increment)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Try Eagle. If the board is less than 100x80mm you can experiment on the free version.

    CadSoft EAGLE PCB Design Software|Support, Tutorials, Shop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Richard_H

    Thanks Richard, that sounds doable, can you tell me which program I should try that on?

    Sorry, I'm new to this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 11 years ago

    You can draw one part of the coil, for example two vias and the wire connection.

    Now select it with GROUP and do a CUT and PASTE to duplicate it. Easiest way is to do this in the command line.

    Some preparation first. Set a MARK in the centre of the coil. Now you can use polar coordinates for duplication.

    What you would do with the mouse  can be done in the comand line, as well.

    The syntax would look like this

    CUT (>CP14 0)   this selects the group and puts into the paste buffer; 
                            similar to a Ctrl+right click onto the polar coords 14 0;  > stands for right click,  C for Ctrl pressed,
                             P for polar

    PASTE R12.5 (P14 12.5)   this places the group rotated by 12.5° in an angle of 12.5° and the same
                                           radius of 14 around the centre

     

    Simply try a bit to get out how it works...

    HTH

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer