Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Double sided PCB design
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 189 subscribers
  • Views 2755 views
  • Users 0 members are here
Related

Double sided PCB design

anishkgt
anishkgt over 9 years ago

Hi all,

 

Since i've started using Eagle, i am now very much familiar with designing one sided. I thought i'd try out double sided.

 

My idea is to design a PCB with a 11pin connector on one side, 8 led on the other and a POT. So that the connector do not come in the way of the LED when mounting the PCB. below is my design just need some advise if the below design is ok as a double sided design before i send it to the fab house.

 

imageimage

  • Sign in to reply
  • Cancel
  • anishkgt
    0 anishkgt over 9 years ago

    Ok i've done as per advised. Would this as i intent ?

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago

    The holes "connected" to R1 do not appear to be plated holes - is this intentional?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago

    Also, use the mirror command on the variable resistor otherwise it won't work in the expected direction (unless you've compensated for that in your wiring which would then need to be corrected too).

    This is assuming you want the variable resistor on the other side.

    Right now from your question it is totally ambiguous if the connector is intended to be on other side, or the remainder components..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago

    Hi George,

     

    It is fortunate here that the components used can be used flipped over, but some components can't

    (e.g. a typical dual-in-line (DIL) microchip would have its connections very wrong if it was soldered on the other side of the board, since the anti-clockwise pin count would become clockwise on the other side - you'd have to bend each pin of the IC to face the other way).

    The real solution is to instruct EAGLE that the part is to be flipped, and it will then correctly handle it.

    To do this, use the 'mirror' command (there is an icon for it in the toolbar on the left side when laying out the PCB).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<