Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum bench power supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 42 replies
  • Answers 20 answers
  • Subscribers 191 subscribers
  • Views 9776 views
  • Users 0 members are here
Related

bench power supply

aster94
aster94 over 9 years ago

hello,

 

I started drawing in eagle this afternoon to make my first home made pbc board for a bench power supply that with an input of 12V/5A will have two output of 12V, 5V, 3.3V and an adjustable voltage (lm317)

the switches are these with ground in the middle

565935243_150.jpg

I hope that the schematic is clear (it is also in the attachments), maybe you could give me some hint or advice about something that i m doing wrong

about the .brd i didn't route it since maybe you will say me to modify my schematic

 

thanks in advance

 

Immagine.png

Attachments:
bps.rar
  • Sign in to reply
  • Cancel
Parents
  • COMPACT
    0 COMPACT over 9 years ago

    I'd definitely put polarity protection at the input.

    Your original design also makes the assumption that you are feeding the board with 12VDC regulated. Is this the case?

    With a linear regulator you can't output 12V from an input of 12V.

    A linear regulator works on the premise that excess power is dissipated as heat but can't absorb heat to boost voltage.

     

    I suggest that you start with a prototype first and test it out to see if it meets your needs.

    1. with input protection.

    2. with a single output.

     

    Once this is working then add your bells and whistles.

    And once this has been done then layout your PCB with sufficiently sized copper traces.

     

    Make sure that the regulators are sufficiently heatsunk to dissipate the unwanted power keeping the regulator temperature within operating bounds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • COMPACT
    0 COMPACT over 9 years ago

    I'd definitely put polarity protection at the input.

    Your original design also makes the assumption that you are feeding the board with 12VDC regulated. Is this the case?

    With a linear regulator you can't output 12V from an input of 12V.

    A linear regulator works on the premise that excess power is dissipated as heat but can't absorb heat to boost voltage.

     

    I suggest that you start with a prototype first and test it out to see if it meets your needs.

    1. with input protection.

    2. with a single output.

     

    Once this is working then add your bells and whistles.

    And once this has been done then layout your PCB with sufficiently sized copper traces.

     

    Make sure that the regulators are sufficiently heatsunk to dissipate the unwanted power keeping the regulator temperature within operating bounds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • aster94
    0 aster94 over 9 years ago in reply to COMPACT

    thanks, i know that i wouldn't be able to output more than Vin-1.15V, i will put the protection diode as you suggested. yes, your assumption is correct, it will be feeded with 12V already regulated

    the heatsink will not be a problem the case will be a panel of alluminium

     

    anyway i edited my previous message before seeing that you had commented