Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum bench power supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 42 replies
  • Answers 20 answers
  • Subscribers 191 subscribers
  • Views 9778 views
  • Users 0 members are here
Related

bench power supply

aster94
aster94 over 9 years ago

hello,

 

I started drawing in eagle this afternoon to make my first home made pbc board for a bench power supply that with an input of 12V/5A will have two output of 12V, 5V, 3.3V and an adjustable voltage (lm317)

the switches are these with ground in the middle

565935243_150.jpg

I hope that the schematic is clear (it is also in the attachments), maybe you could give me some hint or advice about something that i m doing wrong

about the .brd i didn't route it since maybe you will say me to modify my schematic

 

thanks in advance

 

Immagine.png

Attachments:
bps.rar
  • Sign in to reply
  • Cancel
Parents
  • aster94
    0 aster94 over 9 years ago

    finally I'm back! looking a little bit around i found that the lm317 is not the best IC to use in parallel: LM317 in parallel - Answered -> LM2596 circuit question  so i will just be happy with its <1.5A

     

    i draw again the circuit with your precious suggestions:

     

    image

     

    now i have the input of 12V filtered by a 1000uF electrolityc and a 0.1uF ceramic capacitators with:

    -"high" current output with the lm317 (i think that now it is correctly wired)

    -low current output where i could choose between 12/5/3.3 volts

     

    the ammeter/voltmater that i am using is this: https://it.aliexpress.com/item/1pcs-DC-100V-10A-Voltmeter-Ammeter-Blue-Red-LED-Amp-Dual-Digital-Volt-Meter-Gauge-Voltage… as i said before it's the same that jw0752 is using

     

    i think that i could start to draw the board, anyone have any suggestion?

     

    about the power supply from the 220V I was undecided between: https://it.aliexpress.com/item/Free-shipping-2pcs-lot-Power-adapter-EU-UK-AU-US-AC110-220V-to-DC12V-2A-led/1806497704.ht…  and https://it.aliexpress.com/item/New-24W-Regulated-Switching-Power-Supply-LED-Driver-Lighting-Transformer-For-LED-Strip-Li…

    the second one is far away better, isn't it?

     

    EDIT: i was thinking that maybe the ams1117 would stay in a safer position if i use the Vout from the lm7805, correct?

    EDIT2: instead of all these output caps (3,4,5,6,7,8) wouldn't be better if a just put a 100nF ceramic cap before every output? or do you think i will need more filtering?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • aster94
    0 aster94 over 9 years ago

    finally I'm back! looking a little bit around i found that the lm317 is not the best IC to use in parallel: LM317 in parallel - Answered -> LM2596 circuit question  so i will just be happy with its <1.5A

     

    i draw again the circuit with your precious suggestions:

     

    image

     

    now i have the input of 12V filtered by a 1000uF electrolityc and a 0.1uF ceramic capacitators with:

    -"high" current output with the lm317 (i think that now it is correctly wired)

    -low current output where i could choose between 12/5/3.3 volts

     

    the ammeter/voltmater that i am using is this: https://it.aliexpress.com/item/1pcs-DC-100V-10A-Voltmeter-Ammeter-Blue-Red-LED-Amp-Dual-Digital-Volt-Meter-Gauge-Voltage… as i said before it's the same that jw0752 is using

     

    i think that i could start to draw the board, anyone have any suggestion?

     

    about the power supply from the 220V I was undecided between: https://it.aliexpress.com/item/Free-shipping-2pcs-lot-Power-adapter-EU-UK-AU-US-AC110-220V-to-DC12V-2A-led/1806497704.ht…  and https://it.aliexpress.com/item/New-24W-Regulated-Switching-Power-Supply-LED-Driver-Lighting-Transformer-For-LED-Strip-Li…

    the second one is far away better, isn't it?

     

    EDIT: i was thinking that maybe the ams1117 would stay in a safer position if i use the Vout from the lm7805, correct?

    EDIT2: instead of all these output caps (3,4,5,6,7,8) wouldn't be better if a just put a 100nF ceramic cap before every output? or do you think i will need more filtering?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 9 years ago in reply to aster94

    As COMPACT said the regulators need some voltage above their output.

    A good rule of thumb is 2v.

     

    Rather than go ot the 24v supply, many of the power bricks for laptops are 15v and have more than 2A capability.

    That assumes you want to have the adjustable voltage got from zero to 12v.

     

     

    Also a minor difference but if you can the voltmeter input should be on the Output of the ammeter.

    Most ammeters use a small resistance in series and measure the voltage across it to derive the current figure, some are negliglble but others are higher.

     

    You will need to be very disciplined when using the fixed output switch. You really don't want to have 5v (or worse) into a 3v3 device

     

    Otherwise it looks like it will work.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer