Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum bench power supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 42 replies
  • Answers 20 answers
  • Subscribers 191 subscribers
  • Views 9746 views
  • Users 0 members are here
Related

bench power supply

aster94
aster94 over 9 years ago

hello,

 

I started drawing in eagle this afternoon to make my first home made pbc board for a bench power supply that with an input of 12V/5A will have two output of 12V, 5V, 3.3V and an adjustable voltage (lm317)

the switches are these with ground in the middle

565935243_150.jpg

I hope that the schematic is clear (it is also in the attachments), maybe you could give me some hint or advice about something that i m doing wrong

about the .brd i didn't route it since maybe you will say me to modify my schematic

 

thanks in advance

 

Immagine.png

Attachments:
bps.rar
  • Sign in to reply
  • Cancel
Parents
  • jc2048
    0 jc2048 over 9 years ago

    Not sure that the way you have the switch is right. My interpretation of the data would be like this (but I could be wrong):

     

    image

     

    Do you have a meter you can use to see which terminals are joined for the different switch positions?

     

    The switch is only rated to switch 0.3A.

     

    Calculate the power dissipated by each of the regulators before you do the board (you might find they need a heatsinks).

     

    Connect R2 as shown in a 317 datasheet. The way you've got it, though it will work you won't be able to adjust all the way down to the reference voltage.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • aster94
    0 aster94 over 9 years ago in reply to jc2048

    Thanks Jon Clift for your answer,

    I think that your interpretation of the switch is right but to be honest i don t understand what i did wrong. I connected the Ac to ground A1, 2,3,4 are the four different voltages from the ICs.  And from the switch goes out Bc that is the commond ground and a positive voltage from only one of the ICs

     

    I have a multimeter but i ordered the switches only yesterday and i didn t received them yet

     

    About the lm317 i will check the schematic and maybe add some protection diodes, even if i read that they are not necessary

     

    Edit: about the rated current it is 0.5 at 50v so i could reach 2a at 12v and anyway i wouldn t need all these current and the lm7805 and 317 will be scrwed in the metal case,  that is the reason why they are at the edge of the board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to aster94

    the rated current it is 0.5 at 50v so I could reach 2A at 12v

    It doesn't work that way.

     

    The current specifies how much the switch will pass without damaging the contacts.

    The voltage specifies how high a voltage you can apply before you have problems with insulation, arcing over, etc.

     

    At 12v you still have 0.5A.

     

    The voltage/current can be different between AC and DC but it's usually not much.

     

     

    You could change your design.

    If you switched the ADJ pin with different values, you'll have the regulator doing all the work.

    image

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • geralds
    0 geralds over 9 years ago in reply to aster94

    Vincenzo Gibiino wrote:

     

    ...

    In your schematics the middle pin of the potentiometer is not connected, is it correct?

    Is this schematic also good?

     

    Hi,

     

    This is a symbol of a rheostat; An adjustable resistance.

    https://en.wikipedia.org/wiki/Potentiometer#Rheostat

     

    The difference between the rheostat and the potentiometer is that symbolically only two

    connections are connected, because here no voltage divider is necessary.
    So, a potentiometer is an adjustable voltage divider (% upper half //% lower half), a rheostat is not.

    For setting, one end (usually the "hot" end, maximum stop) and the slider are wired.
    (Usual, cold end = left, hot end = to the right of the stop, looking forward to the axis)

    This also has the disadvantage in the case of the adjustable resistance that when the slider is interrupted,

    e.g. by dust inclusions, or jumping, the entire resistance is interrupted.
    Therefore, the "cold end" of the adjustable resistor is also connected for safety reasons.
    Then, in the case of the interruption, at least the total resistance value has the connection.
    In this way, this circuit can still control, in this case only with the maximum resistance value.
    In the case of the rheostat, the regulation would fail.

     

    The schematic have fundamental errors (sorry).

     

    Best Regards,

    Gerald

    ----

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • geralds
    0 geralds over 9 years ago in reply to aster94

    Vincenzo Gibiino wrote:

     

    ...

    In your schematics the middle pin of the potentiometer is not connected, is it correct?

    Is this schematic also good?

     

    Hi,

     

    This is a symbol of a rheostat; An adjustable resistance.

    https://en.wikipedia.org/wiki/Potentiometer#Rheostat

     

    The difference between the rheostat and the potentiometer is that symbolically only two

    connections are connected, because here no voltage divider is necessary.
    So, a potentiometer is an adjustable voltage divider (% upper half //% lower half), a rheostat is not.

    For setting, one end (usually the "hot" end, maximum stop) and the slider are wired.
    (Usual, cold end = left, hot end = to the right of the stop, looking forward to the axis)

    This also has the disadvantage in the case of the adjustable resistance that when the slider is interrupted,

    e.g. by dust inclusions, or jumping, the entire resistance is interrupted.
    Therefore, the "cold end" of the adjustable resistor is also connected for safety reasons.
    Then, in the case of the interruption, at least the total resistance value has the connection.
    In this way, this circuit can still control, in this case only with the maximum resistance value.
    In the case of the rheostat, the regulation would fail.

     

    The schematic have fundamental errors (sorry).

     

    Best Regards,

    Gerald

    ----