Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum bench power supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 42 replies
  • Answers 20 answers
  • Subscribers 191 subscribers
  • Views 9746 views
  • Users 0 members are here
Related

bench power supply

aster94
aster94 over 9 years ago

hello,

 

I started drawing in eagle this afternoon to make my first home made pbc board for a bench power supply that with an input of 12V/5A will have two output of 12V, 5V, 3.3V and an adjustable voltage (lm317)

the switches are these with ground in the middle

565935243_150.jpg

I hope that the schematic is clear (it is also in the attachments), maybe you could give me some hint or advice about something that i m doing wrong

about the .brd i didn't route it since maybe you will say me to modify my schematic

 

thanks in advance

 

Immagine.png

Attachments:
bps.rar
  • Sign in to reply
  • Cancel
Parents
  • aster94
    0 aster94 over 9 years ago

    thanks again to mcb1 and COMPACT, I would like to say that, as I wrote before, I don't have any tool (except the voltmeter at 3$), but I know that linear regulator dissipate the excess power as heat and that dc-dc regulator are more efficient. I am making this simple bench power supply just for hobby to improve my abilities, especially about the pcb making (drawing, printing, ectching ecc) and because sometimes I need one

     

    I looked on google for the S100, do you mean this:  http://www.s100computers.com/My%20System%20Pages/The%20Box/Linear%20Power%20Supply%20in%20Box.jpg  my first purpose is to do something on "my own", not to buy a ready to use one

     

    deliberately have polarised capacitors attached back to front or use capacitors beyond their rated working voltage

     

     

    mmm I will try if this is not a smart way to try to kill me image ahahah obviosly I'm joking

     

    here there is the -I think- last version, as you adviced I

    1. put the protection diode on the input
    2. changed the simbol for the imput since i will use a dc plug (I'm not sure if it is correctly wired)
    3. moved the ams1117 after the lm7805
    4. reduced the number of caps
    5. moved the voltmeter input
    6. added a lm7812

     

     

    image

     

    the cap that i will use:

    C1- electrolytic 2,200 - 4,700 uF, 25V

    C2,4,6 - ceramic 0.1uF , 25V

    C3,5 - electrolytic 1/10 of C1 (i read it somewhere I don't know if it is correct), 25V

     

    next week I will start making the board, I attached the schematics and a really really first version of the board (i just put the component where they should be more or less), my goal is to make it single layer (since i am making it home), the sizes on the edges are the maximum that i could use image

     

    NOTE: in the board the first swith is not present because it will be on the front panel not on the pcb

    Attachments:
    bench power supply.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 9 years ago in reply to aster94

    Hi,

     

    please check your circuit!

    image

     

    Best Regards,

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • aster94
    0 aster94 over 9 years ago in reply to geralds

    Gerald, i own you a coffe

     

    image

     

    it was wrong since the first time i draw it and i never saw it... ops...

    now i think everythink is ok image tomorrow i will finish the .brd and than i will ask a friend who have all the etching stuff!

    while i am here, on eagle i always see the shortest connection thanks to the rats net, is possible to see the connection in order as i draw in the schematic? i don't know if i explained me in a good way, i mean that i would like to see the dc input going to the diode than to the swith and so on

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • aster94
    0 aster94 over 9 years ago in reply to geralds

    Gerald, i own you a coffe

     

    image

     

    it was wrong since the first time i draw it and i never saw it... ops...

    now i think everythink is ok image tomorrow i will finish the .brd and than i will ask a friend who have all the etching stuff!

    while i am here, on eagle i always see the shortest connection thanks to the rats net, is possible to see the connection in order as i draw in the schematic? i don't know if i explained me in a good way, i mean that i would like to see the dc input going to the diode than to the swith and so on

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • aster94
    0 aster94 over 9 years ago in reply to geralds

    Gerald Schwarz ha scritto:
    ) The plug can not be used for 5A, at least only special types of plug.

    at the end i will just use 1.5A, i think it would be able to handle them (wikipedia says 2A)

     

    ) There is a better solution for polarity reversal protection, eg with a P-channel MOSFET.
    ) A filter (C-L-C at the input) should be inserted, especially bypass capacitors should be installed in the right places.

    I am an hobbyist making my first power supply, I would like to do something veeeery simple, i found these solution on google and they don't seem to difficult to apply: https://forum.allaboutcircuits.com/threads/pi-filter-clc.2687/ and http://lh4.googleusercontent.com/-uZWaEG-Yhn4/UAXdcxfPDLI/AAAAAAAAET0/SWL6YD6HwYg/s398/input-protect.png  so I would go with your better solutions for my next board but for now i will just use the two capacitor for filter the input


    ) The supply for the panel meter (V / A) I would solve differently (what kind of panel meter have you?).

    this: https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Fit.aliexpress.com%2Fitem%2F1pcs-DC-100V-10A-Vol…

     

    ) The switch at the output I would make with a rotary switch and relay, because the relay contacts can handle the current.
    ) The sliding switch described above is more suitable for signal currents.
    ) Or, even better, direct all outputs directly to the terminals, so you can use all outputs at the same time.

    at the end i think that i would do as you and COMPACT said,having all outputs free is better

     

    ) The part with the LM317 should be modified.
    For setting, one end (usually the "hot" end, maximum stop) and the slider are wired.
    (Usual, cold end = left, hot end = to the right of the stop, looking forward to the axis)

    I am not sure to have understood where the problem is: do i just need to invert the hot and cold end of the pot?

     

    edit: added new shematics at the end of this topic

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to aster94

    You'll find that having both +5V and +3V3 simultaneously handy to have.

    If you're going to have low impedance regulator input capacitor like C2 you should have one for each regulator.

    Apparently, the shorter the distance from the voltage regulator the better.

     

    Lose the slide switch and use an appropriately rated toggle switch.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • geralds
    0 geralds over 9 years ago in reply to aster94

    Hi,

     

    My pleasure.
    Please wait a bit for etching, because the circuit diagram has some fundamental errors.
    For example:
    ) The plug can not be used for 5A, at least only special types of plug.
    ) There is a better solution for polarity reversal protection, eg with a P-channel MOSFET.
    ) A filter (C-L-C at the input) should be inserted, especially bypass capacitors should be installed in the right places.
    ) The supply for the panel meter (V / A) I would solve differently (what kind of panel meter have you?).
    ) The switch at the output I would make with a rotary switch and relay, because the relay contacts can handle the current.
    ) The sliding switch described above is more suitable for signal currents.
    ) Or, even better, direct all outputs directly to the terminals, so you can use all outputs at the same time.
    ) The part with the LM317 should be modified.

     

    There was some hints for checking the schematic.

     

    Best Regards,

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer