Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum bench power supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 42 replies
  • Answers 20 answers
  • Subscribers 191 subscribers
  • Views 9734 views
  • Users 0 members are here
Related

bench power supply

aster94
aster94 over 9 years ago

hello,

 

I started drawing in eagle this afternoon to make my first home made pbc board for a bench power supply that with an input of 12V/5A will have two output of 12V, 5V, 3.3V and an adjustable voltage (lm317)

the switches are these with ground in the middle

565935243_150.jpg

I hope that the schematic is clear (it is also in the attachments), maybe you could give me some hint or advice about something that i m doing wrong

about the .brd i didn't route it since maybe you will say me to modify my schematic

 

thanks in advance

 

Immagine.png

Attachments:
bps.rar
  • Sign in to reply
  • Cancel
Parents
  • aster94
    0 aster94 over 9 years ago

    follow up:

    i hope that with this post i won't be seen as arrogant since I didn't use the schematic from @geralds

    His draw is obviously far away better than mine, but my main desire was to do this bench power supply on my own

     

    I completed the board in only one side, i used extra isolation for the ground plane than needed since i m not sure about our homemade etching quality

     

    image

     

    Now i will just have to wait for the 7812 then i will finish it image

    P.S: I know that the ground plane is not perfect near the lm317's outputs i will put a jumper

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to aster94

    Vincenzo,

     

    You seem to be focused on ancillary considerations and not the primary considerations as I've tried to lead you.

     

    Don't concern yourself about using power plane fills but get the essentials in order first.

     

    Here are some observations.

     

    1. PCB traces are too thin; they need to be thick enough to handle the envisaged current and be thick enough firstly to avoid acting as an unwanted fuse and handling the envisaged load.

     

    2.Your low impedance, small capacitance (100n) capacitors for the voltage regulator outputs are far too far away from the voltage regulators; ideally they should be adjacent.

     

    Have a look at Steve Ciarcia's Circuit Cellar How to build your own Z80 computer book which is available online which has a great section on power supplies for beginners.

     

    https://books.google.com.au/books?id=mVQnFgWzX0AC&printsec=frontcover&source=gbs_ge_summary_r&cad=0#v=onepage&q&f=false

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • aster94
    0 aster94 over 9 years ago in reply to COMPACT

    "You seem to be focused on ancillary considerations and not the primary considerations as I've tried to lead you."

    you are right i was so focused to connect all the components in the board that i forgot to give an appropriate width to the tracks, I used this calculator: The CircuitCalculator.com Blog » PCB Trace Width Calculator  and i used 50mil for the main power lines before the ICs and 32mil after the ICs since techinically the max amp after them should be <1.5 amp

     

    about the capacitors i really misunderstood a previous post, i thought that they had to stay as near as possible to the outputs....

    now i think it is correct

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • aster94
    0 aster94 over 9 years ago in reply to COMPACT

    "You seem to be focused on ancillary considerations and not the primary considerations as I've tried to lead you."

    you are right i was so focused to connect all the components in the board that i forgot to give an appropriate width to the tracks, I used this calculator: The CircuitCalculator.com Blog » PCB Trace Width Calculator  and i used 50mil for the main power lines before the ICs and 32mil after the ICs since techinically the max amp after them should be <1.5 amp

     

    about the capacitors i really misunderstood a previous post, i thought that they had to stay as near as possible to the outputs....

    now i think it is correct

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • geralds
    0 geralds over 9 years ago in reply to aster94

    Hi,

     

    fine, congratulations!

     

    A little bit:

    1) place the output connectors and poti also the V-regulators a bit to inside of the board, then you have a closed GND plane with this polygon.

    Then you don't need wire jumpers.

     

    2) turn the input plug backwards to the IC side then you can make a small enclosure around the PCB that have on the front- and backside the mounting parts but not on the l/r sides.

     

    The 100n bypass capacitors have mounting so close to the ICs as you can. They are ceramic capacitors, withstanding > 50V.

     

    Best Regards,

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer