Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum AC to DC Power Supply Design
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 192 subscribers
  • Views 2105 views
  • Users 0 members are here
  • energy_power
Related

AC to DC Power Supply Design

e14 Contributor
e14 Contributor over 9 years ago

Afternoon all,

 

Late on a Friday, I am clearly making some sort of simple error but I am blind to it.

 

Please see the circuit below.  I have soldered it up and it isn't working.  I get 36VDC on what should be the regulated 12V rail and a little over 1VDC on the 5VDC rail.

 

Any ideas, please?  I should add that if I remove the transformer and supply 18VDC from my bench PSU then everything works fine, even after the 36V spike which is over the LT3501 max so I *think* the regulator is fine.

 

The number above the transformer is a UK Farnell product code.  It is a 2x 9V transformer with the secondaries wired in series to give 18V.

 

Cheers,

 

Simon

 

PS: Context; it is a power supply for a rPi which is controlling, among other things, some 12V RGB LEDs.

image

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Simon,

    I assume you have check the Data sheet for some guidance but just in case here is a link to it:

     

    http://datasheet.octopart.com/LT3501EFE%23PBF-Linear-Technology-datasheet-17021123.pdf

     

    Some problem in the voltage dividers tied to FB-1 and FB-2 could have this effect but I have never worked with this circuit. Check out the sample circuit in the Data Sheet as it may be clearer than the schematic you have above though the resistor values may not be the same as they are showing a different set of regulated voltages.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi Simon,

    I assume you have check the Data sheet for some guidance but just in case here is a link to it:

     

    http://datasheet.octopart.com/LT3501EFE%23PBF-Linear-Technology-datasheet-17021123.pdf

     

    Some problem in the voltage dividers tied to FB-1 and FB-2 could have this effect but I have never worked with this circuit. Check out the sample circuit in the Data Sheet as it may be clearer than the schematic you have above though the resistor values may not be the same as they are showing a different set of regulated voltages.

     

    John