Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Am I connecting electrically two wires if I connect 2 lines
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 1514 views
  • Users 0 members are here
Related

Am I connecting electrically two wires if I connect 2 lines

mikelima
mikelima over 8 years ago

Suppose this situation. I have 3 resistors in parallel. I draw a line from resistor 1 to 3, like the picture below.

 

image

 

Are these 4 resistors connected electrically of do I need to put a junction like this?

 

image

My intention is to convert this into a PCB later.

 

Another question... are two lines that touch connected electrically or do I have to put a junction?

 

image

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Mike,

     

    Although what you've done can work fine, I think you're using the 'Wire' tool from the tool palette. It has the visible symptom that there is no blob automatically created when a wire terminated on top of another wire.

    The 'Wire' tool should not be used as a result, and instead the 'Net' tool should be used from that tool palette. When that tool is used, there is no need to ever place a manual junction.

    EAGLE being what it is, allows you to manually do these things as an option, but is unnecessary if you use the Net tool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago

    Hi Mike,

     

    Although what you've done can work fine, I think you're using the 'Wire' tool from the tool palette. It has the visible symptom that there is no blob automatically created when a wire terminated on top of another wire.

    The 'Wire' tool should not be used as a result, and instead the 'Net' tool should be used from that tool palette. When that tool is used, there is no need to ever place a manual junction.

    EAGLE being what it is, allows you to manually do these things as an option, but is unnecessary if you use the Net tool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer