I've just upgraded to 5.7, and I see that this has been changed:
- Switching between windows with Alt+0, Alt+1 etc. has been disabled on
the Mac OS X platform, because on some localized keyboard layouts these
key combinations are already used otherwise.
Is there either a way to reactivate them, or is there a command that I can use ASSIGN to set up a key switch myself to do this?
I've spent quite a while looking through the help, and also internet searches, but I guess it's too modern for the latter! I was hoping that the WINDOW command might do it, but it doesn't seem to switch between the different windows (only sections in the current window). I can switch to the board by using the BOARD command, but I haven't found a way to switch back to the schematic (or even control panel).
If there isn't, then it's just become exceptionally clumsy switching between windows, as the menu option is the only way - and this is very cumbersome if you've got two large screens. It feels like a huge step backwards.
I have to admit that there were issues with it on 5.6 anyway - such as switching the window, and then using the scroll wheel would cause the original window to zoom in/out, rather than the one I've just switched to; also, the numbering would sometimes change depending on whether you'd opened a board, schematic, library editor or help...