Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Switching windows on MacOS X and Eagle 5.7
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 190 subscribers
  • Views 1458 views
  • Users 0 members are here
  • keyboard
  • window
  • switch
  • macos_x
Related

Switching windows on MacOS X and Eagle 5.7

e14 Contributor
e14 Contributor over 16 years ago

I've just upgraded to 5.7, and I see that this has been changed:

 

  - Switching between windows with Alt+0, Alt+1 etc. has been disabled on
    the Mac OS X platform, because on some localized keyboard layouts these
    key combinations are already used otherwise.

 

Is there either a way to reactivate them, or is there a command that I can use ASSIGN to set up a key switch myself to do this?

 

I've spent quite a while looking through the help, and also internet searches, but I guess it's too modern for the latter! I was hoping that the WINDOW command might do it, but it doesn't seem to switch between the different windows (only sections in the current window). I can switch to the board by using the BOARD command, but I haven't found a way to switch back to the schematic (or even control panel).

 

If there isn't, then it's just become exceptionally clumsy switching between windows, as the menu option is the only way - and this is very cumbersome if you've got two large screens. It feels like a huge step backwards.

 

I have to admit that there were issues with it on 5.6 anyway - such as switching the window, and then using the scroll wheel would cause the original window to zoom in/out, rather than the one I've just switched to; also, the numbering would sometimes change depending on whether you'd opened a board, schematic, library editor or help...

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Greetings Jason,

     

    I will look into this for you.

     

    On the Windows platform, hitting Alt+W still brings me to the "Windows" tool bar, from there I can still hit  "1" or "2" or "3" etc. and select a window

     

    This is one more keystroke but it does get me to other windows with my left hand.

     

    Will this approach work in MacOS X?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • atomar
    0 atomar over 16 years ago in reply to e14 Contributor

    Hello Jacob,

    I am also not sure about the MacOS X, but in Windows OS you can use Alt + Tab  key to switch between windows without any any further clicks, it work with Eagle as well.

     

    Just press Alt + Tab and you will get a small pop up window where you can  select any window but just pressing Tab key ( without releasing Alt key), you can switch to any window without any clicks.

     

    Its a standard Windows key shortcut and work in almost all software's.

     

    Ankur

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to atomar

    Many thanks for those that replied overnight (well, it was overnight for me!)

     

    I think that Richard's answer is the correct one - I'll try the edit .brd and edit .sch tonight. Unfortunately, it doesn't give me an option to go to back to the Control Panel, which I occasionally need to do because I always trim my libraries down to a minimum, and only add them back in when I discover I need an object in a library that I didn't enable. Luckily the "occasionally" aspect of this means its probably okay (for the time being). And I don't do component editing that often.

     

    I am a Windows and MacOS Developer, so I'm familiar with the decisions as to why it was done that way - it just would've been nice to have an eaglerc option to revert it! I use a custom keymap which is identical to the Windows one, so I don't have that problem.

     

    Alt-W followed by number isn't a nomenclature that MacOS X uses (although there may be another way to do it; never really thought about it) - and Alt-Tab, while there is a MacOS X equivalent, it only switches between programs, and not windows within a program. I know that both will work on Windows.

     

    I also know that MacOS X Eagle users are almost certainly in a minority image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to KennyMillar

    It's a little more subtle than that:

     

    When you use a PC with a French keyboard, there are two Alt keys - the left one is Alt, the right is Alt-Gr.

     

    To enter characters like "{" and "[", you use Alt-Gr with the relevant number key, whereas Alt with the number doesn't really do anything unless the application itself understands those key presses.

     

    On MacOS, both keys act like Alt-Gr, so pressing either Alt key you're meant to get "{" and "[".

     

    The problem is that CadSoft had a rather handy way of switching between windows with the Alt keys - which works fine on a PC due the distinction between the two Alt keys. However, on MacOS, this doesn't work terribly well if you need to create ULPs, since you'd find yourself switching between windows unexpectedly.

     

    The possible solutions I can come up with are:

     

    - Work out which of the Alt keys are being pressed, so it acts like the PC.

     

    Unfortunately, this isn't really a good solution since users may be used to pressing the left Alt key instead of the right Alt key to get their characters.

     

    - Disable window switching when in a text editor window

     

    This will work, but it is a bit ... clunky.

     

    - Make it a configurable option

     

    Again, this will work, but means there isn't an option for some keyboard types to switch windows.

     

    - Make the key combinations themselves configurable

     

    This would be the best solution (IMHO), but is a lot more development work.

     

    Note that the Fn key itself has no relevance on this at all; that mainly controls the operation of the function keys, and not the number keys (I've set mine up so the Exposé et. al. keys need Fn pressed). To the best of my knowledge, no amount of changes to the system configuration would actually allow the left Alt to be different to the right Alt, and the "{", "[" characters aren't system functions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KennyMillar
    0 KennyMillar over 16 years ago in reply to Richard_H

    Hi Richard,

     

    Thats good to know.

    I really like Eagle, sorry if my post sounded a bit pompous!

     

    -Kenny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 16 years ago in reply to KennyMillar

     

    I really think that CadSoft should have left this feature enabled and given the users advice on how to use the system preferences to get what they need. Now the needs of the few are outnumbering the needs of the many. Cadsoft should have empowered the user, rather than cripple the software.

     

     

    I will forward this subject to our development people again. Maybe we can find a good solution for the future.

     

    -Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KennyMillar
    0 KennyMillar over 16 years ago in reply to e14 Contributor
    I am a Windows and MacOS Developer, so I'm familiar with the decisions as to why it was done that way

     

     

    You know, Apple know about these things, thats why in system preferences on Mac OS X you have to choice to use either the system functions for the keys or the applications function. (Then you can access the 'system' functions by using the FN button).

     

    Mac OS X also allows the user to re-assign system keys which clash with application shortcuts.

     

    I really think that CadSoft should have left this feature enabled and given the users advice on how to use the system preferences to get what they need. Now the needs of the few are outnumbering the needs of the many. Cadsoft should have empowered the user, rather than cripple the software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Richard_H

    Yup - I've read that, but sometimes you become a bit blind and miss something image

     

    Nothing else has leapt out at me as being a change in the way I work (the migration of the "As PDF" button to a drop-down had me worried that the PDF generation had been altered, and my PDF reader [which I use to group up several PCBs, annotate and then print for photo etching] wouldn't be able to cope with it, but it's as happy as it was beforehand).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 16 years ago in reply to e14 Contributor

    Hi again,

     

    all the differences between EAGLE versions are documented in the file UPDATE in eagle's doc folder.

    Have fun!

     

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Richard_H
    0 Richard_H over 16 years ago in reply to e14 Contributor

    Hi again,

     

    all the differences between EAGLE versions are documented in the file UPDATE in eagle's doc folder.

    Have fun!

     

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Richard_H

    Yup - I've read that, but sometimes you become a bit blind and miss something image

     

    Nothing else has leapt out at me as being a change in the way I work (the migration of the "As PDF" button to a drop-down had me worried that the PDF generation had been altered, and my PDF reader [which I use to group up several PCBs, annotate and then print for photo etching] wouldn't be able to cope with it, but it's as happy as it was beforehand).