I saw their is a make-symbol-device-package-bsdl.ulp, and tried some bsdl file. very nice.
but it seems don't support ibis file, is this true?
I saw their is a make-symbol-device-package-bsdl.ulp, and tried some bsdl file. very nice.
but it seems don't support ibis file, is this true?
Hi,
The ULP you have mentioned above helps the user to generate the entire device including the symbol and package by just a click of a button. It is indeed a neat feature.
But, I don't think it can generate a IBIS file. An IBIS is a behavioural model that describes the electrical characteristics of the digital inputs and outputs of a device. An IBISmodel consists of tabular data made of current, voltage and RLC parasictic values in the input and output pins. Such models are obtained by gathering data in Simulations or from bench measurements. Since there is no simulation data generated from executing this ulp, an IBIS model probably cannot be generated.
Hope this has answered your question.
Richard, Jorge any comments?
Regards,
Jaya
Hi,
The ULP you have mentioned above helps the user to generate the entire device including the symbol and package by just a click of a button. It is indeed a neat feature.
But, I don't think it can generate a IBIS file. An IBIS is a behavioural model that describes the electrical characteristics of the digital inputs and outputs of a device. An IBISmodel consists of tabular data made of current, voltage and RLC parasictic values in the input and output pins. Such models are obtained by gathering data in Simulations or from bench measurements. Since there is no simulation data generated from executing this ulp, an IBIS model probably cannot be generated.
Hope this has answered your question.
Richard, Jorge any comments?
Regards,
Jaya
but ibis file include the pin define and package, not only current, voltage and etc..
such as this section from lxt971a_b_mii_3_32.ibs file:
[Component] lxt971a_b_mii_3_3
[Manufacturer] CORTINA_SYSTEMS,_INC.
[Package]
| 64-Pin LQFP Package
| variable typ min max
R_pkg 1.2m NA NA
L_pkg 6nH NA NA
C_pkg 1.1pF NA NA
|
[Pin] signal_name model_name R_pin L_pin C_pin
B1 REFCLK/XI INPUT
C1 XO 3X_OUTPUT
D3 MDDIS INPUT
C2 RESET INPUT
D1 TXSLEW0 INPUT
D2 TXSLEW1 INPUT
D4 GND GND
E5 VCCIO POWER
B7 NC NC
C7 NC NC
E3 GND GND
E1 ADDR0 INPUT
E2 ADDR1 INPUT
F2 ADDR2 INPUT
F1 ADDR3 INPUT
G1 ADDR4 INPUT
H1 RBIAS INPUT
E4 GND GND
H2 TPFOP NC
H3 TPFON NC
G3 VCCA POWER
G4 VCCA POWER
H4 TPFIP INPUT
H5 TPFIN INPUT
F3 GND GND
G2 SD/TP INPUT
F5 TDI INPUT
G5 TDO 6X_OUTPUT
F6 TMS INPUT
G6 TCK INPUT
H6 TRST INPUT
H7 SLEEP INPUT
H8 PAUSE INPUT
G8 TEST0 INPUT
G7 TEST1 INPUT
F8 LED/CFG3 6X_INPUT_OUTPUT
F7 LED/CFG2 6X_INPUT_OUTPUT
E6 LED/CFG1 6X_INPUT_OUTPUT
E8 PWRDWN INPUT
D5 VCCIO POWER
F4 GND GND
D8 MDIO 1X_IN_OUT
E7 MDC INPUT
D7 NC NC
D6 RXD3 3X_OUTPUT
C8 RXD2 3X_OUTPUT
B8 RXD1 3X_OUTPUT
A8 RXD0 3X_OUTPUT
A7 RX_DV 3X_OUTPUT
C6 GND GND
A6 VCCD POWER
B6 RX_CLK 3X_OUTPUT
A5 RX_ER 3X_OUTPUT
B5 TX_ER INPUT
C5 TX_CLK 3X_OUTPUT
B4 TX_EN INPUT
A4 TXD0 INPUT
C4 TXD1 INPUT
B3 TXD2 INPUT
A3 TXD3 INPUT
C3 GND GND
B2 COL 3X_OUTPUT
A2 CRS 3X_OUTPUT
A1 MDINT 1X_OPEN_DRAIN
|
|
[Diff Pin] inv_pin vdiff tdelay_typ tdelay_min tdelay_max
H4 H5 1.2V NA NA NA
|
|
so I think it is can be archieved if official do some extend for make-symbol-device-package-bsdl.ulp.
Hi Jaya,
your answer is absolutely correct.
Regards,
Richard