Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum is the make-symbol-device-package-bsdl.ulp support ibis?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 189 subscribers
  • Views 1396 views
  • Users 0 members are here
Related

is the make-symbol-device-package-bsdl.ulp support ibis?

huayuliang
huayuliang over 16 years ago

I saw their is a make-symbol-device-package-bsdl.ulp, and tried some bsdl file. very nice.

but it seems don't support ibis file, is this true?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Hi,

     

    The ULP you have mentioned above helps the user to generate the entire device including the symbol and package by just a click of a button. It is indeed a neat feature.

    But, I don't think it can generate a IBIS file. An IBIS is a behavioural model that describes the electrical characteristics of the digital inputs and outputs of a device. An IBISmodel consists of tabular data made of current, voltage and RLC parasictic values in the input and output pins. Such models are obtained by gathering data in Simulations or from bench measurements. Since there is no simulation data generated from executing this ulp, an IBIS model probably cannot be generated.

     

    Hope this has answered your question.

    Richard, Jorge any comments?

     

    Regards,

    Jaya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • huayuliang
    0 huayuliang over 16 years ago in reply to e14 Contributor

    but ibis file include the pin define and package, not only current, voltage and etc..


    such as this section from lxt971a_b_mii_3_32.ibs file:

     

    [Component]      lxt971a_b_mii_3_3
    [Manufacturer]   CORTINA_SYSTEMS,_INC.
    [Package]
    | 64-Pin LQFP Package
    | variable       typ                min           max
    R_pkg            1.2m               NA            NA
    L_pkg            6nH                NA            NA
    C_pkg            1.1pF              NA            NA
    |
    [Pin]         signal_name          model_name       R_pin     L_pin    C_pin
      B1       REFCLK/XI                     INPUT  
      C1              XO                 3X_OUTPUT  
      D3           MDDIS                     INPUT  
      C2           RESET                     INPUT  
      D1         TXSLEW0                     INPUT  
      D2         TXSLEW1                     INPUT  
      D4             GND                       GND  
      E5           VCCIO                     POWER  
      B7              NC                        NC  
      C7              NC                        NC  
      E3             GND                       GND  
      E1           ADDR0                     INPUT  
      E2           ADDR1                     INPUT  
      F2           ADDR2                     INPUT  
      F1           ADDR3                     INPUT  
      G1           ADDR4                     INPUT  
      H1           RBIAS                     INPUT  
      E4             GND                       GND  
      H2           TPFOP                        NC  
      H3           TPFON                        NC  
      G3            VCCA                     POWER  
      G4            VCCA                     POWER  
      H4           TPFIP                     INPUT  
      H5           TPFIN                     INPUT  
      F3             GND                       GND  
      G2           SD/TP                     INPUT  
      F5             TDI                     INPUT  
      G5             TDO                 6X_OUTPUT  
      F6             TMS                     INPUT  
      G6             TCK                     INPUT  
      H6            TRST                     INPUT  
      H7           SLEEP                     INPUT  
      H8           PAUSE                     INPUT  
      G8           TEST0                     INPUT  
      G7           TEST1                     INPUT  
      F8        LED/CFG3           6X_INPUT_OUTPUT  
      F7        LED/CFG2           6X_INPUT_OUTPUT  
      E6        LED/CFG1           6X_INPUT_OUTPUT  
      E8          PWRDWN                     INPUT  
      D5           VCCIO                     POWER  
      F4             GND                       GND  
      D8            MDIO                 1X_IN_OUT  
      E7             MDC                     INPUT  
      D7              NC                        NC  
      D6            RXD3                 3X_OUTPUT  
      C8            RXD2                 3X_OUTPUT  
      B8            RXD1                 3X_OUTPUT  
      A8            RXD0                 3X_OUTPUT  
      A7           RX_DV                 3X_OUTPUT  
      C6             GND                       GND  
      A6            VCCD                     POWER  
      B6          RX_CLK                 3X_OUTPUT  
      A5           RX_ER                 3X_OUTPUT  
      B5           TX_ER                     INPUT  
      C5          TX_CLK                 3X_OUTPUT  
      B4           TX_EN                     INPUT  
      A4            TXD0                     INPUT  
      C4            TXD1                     INPUT  
      B3            TXD2                     INPUT  
      A3            TXD3                     INPUT  
      C3             GND                       GND  
      B2             COL                 3X_OUTPUT  
      A2             CRS                 3X_OUTPUT  
      A1           MDINT                1X_OPEN_DRAIN  
    |
    |
    [Diff Pin]     inv_pin    vdiff    tdelay_typ      tdelay_min        tdelay_max
      H4           H5         1.2V     NA              NA                NA
    |
    |

     

    so I think it is can be archieved if official do some extend for make-symbol-device-package-bsdl.ulp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • huayuliang
    0 huayuliang over 16 years ago in reply to e14 Contributor

    but ibis file include the pin define and package, not only current, voltage and etc..


    such as this section from lxt971a_b_mii_3_32.ibs file:

     

    [Component]      lxt971a_b_mii_3_3
    [Manufacturer]   CORTINA_SYSTEMS,_INC.
    [Package]
    | 64-Pin LQFP Package
    | variable       typ                min           max
    R_pkg            1.2m               NA            NA
    L_pkg            6nH                NA            NA
    C_pkg            1.1pF              NA            NA
    |
    [Pin]         signal_name          model_name       R_pin     L_pin    C_pin
      B1       REFCLK/XI                     INPUT  
      C1              XO                 3X_OUTPUT  
      D3           MDDIS                     INPUT  
      C2           RESET                     INPUT  
      D1         TXSLEW0                     INPUT  
      D2         TXSLEW1                     INPUT  
      D4             GND                       GND  
      E5           VCCIO                     POWER  
      B7              NC                        NC  
      C7              NC                        NC  
      E3             GND                       GND  
      E1           ADDR0                     INPUT  
      E2           ADDR1                     INPUT  
      F2           ADDR2                     INPUT  
      F1           ADDR3                     INPUT  
      G1           ADDR4                     INPUT  
      H1           RBIAS                     INPUT  
      E4             GND                       GND  
      H2           TPFOP                        NC  
      H3           TPFON                        NC  
      G3            VCCA                     POWER  
      G4            VCCA                     POWER  
      H4           TPFIP                     INPUT  
      H5           TPFIN                     INPUT  
      F3             GND                       GND  
      G2           SD/TP                     INPUT  
      F5             TDI                     INPUT  
      G5             TDO                 6X_OUTPUT  
      F6             TMS                     INPUT  
      G6             TCK                     INPUT  
      H6            TRST                     INPUT  
      H7           SLEEP                     INPUT  
      H8           PAUSE                     INPUT  
      G8           TEST0                     INPUT  
      G7           TEST1                     INPUT  
      F8        LED/CFG3           6X_INPUT_OUTPUT  
      F7        LED/CFG2           6X_INPUT_OUTPUT  
      E6        LED/CFG1           6X_INPUT_OUTPUT  
      E8          PWRDWN                     INPUT  
      D5           VCCIO                     POWER  
      F4             GND                       GND  
      D8            MDIO                 1X_IN_OUT  
      E7             MDC                     INPUT  
      D7              NC                        NC  
      D6            RXD3                 3X_OUTPUT  
      C8            RXD2                 3X_OUTPUT  
      B8            RXD1                 3X_OUTPUT  
      A8            RXD0                 3X_OUTPUT  
      A7           RX_DV                 3X_OUTPUT  
      C6             GND                       GND  
      A6            VCCD                     POWER  
      B6          RX_CLK                 3X_OUTPUT  
      A5           RX_ER                 3X_OUTPUT  
      B5           TX_ER                     INPUT  
      C5          TX_CLK                 3X_OUTPUT  
      B4           TX_EN                     INPUT  
      A4            TXD0                     INPUT  
      C4            TXD1                     INPUT  
      B3            TXD2                     INPUT  
      A3            TXD3                     INPUT  
      C3             GND                       GND  
      B2             COL                 3X_OUTPUT  
      A2             CRS                 3X_OUTPUT  
      A1           MDINT                1X_OPEN_DRAIN  
    |
    |
    [Diff Pin]     inv_pin    vdiff    tdelay_typ      tdelay_min        tdelay_max
      H4           H5         1.2V     NA              NA                NA
    |
    |

     

    so I think it is can be archieved if official do some extend for make-symbol-device-package-bsdl.ulp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • huayuliang
    0 huayuliang over 16 years ago in reply to e14 Contributor

    sorry for my bad english make you misunderstanding.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Oliver

    Hi Huayuliang,

     

    sorry, i think i got your first question wrong. From your very first question I inferred that you were asking if an IBIS file could be generated from the "make-symbol-device-bsdl.ulp". But I guess, it was the other way round. Yes, it is certainly possible. The IBIS file contains the Pin number and the signal name, so a ULP can be written which imports the ibis file, reads the pin number, signal name and would generate the symbol/package required.

     

    Regards,

    Jaya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Oliver
    0 Oliver over 16 years ago in reply to huayuliang

    Do you mean that ULP can pick up the Pin number and Signal name from ibis file? and create the symbol?

     

    It is a good ideal, and some EDA tool can support symbol creation from external spreadsheet.