Hello,
I need help in creating a footprint for the inductor, PM2110 and diode, POWERDI123. Has anybody created any for these devices and is willing to share.
Thanks.
Regards,
Jaya
Hello,
I need help in creating a footprint for the inductor, PM2110 and diode, POWERDI123. Has anybody created any for these devices and is willing to share.
Thanks.
Regards,
Jaya
I did a quick search for "2110" and "123" using my Eagle search tool (which only covers the 5.6 standard libraries at this moment in time).
The only packages with "2110" in their name were SIMM connectors, and with "2110" in their description were mainly about RC6123 wave/reflow soldering packages, and some relays.
The only packages with "123" in their name were SOD-123 (probably not the same footprint), and "123" in their description wa sa 256-pin PBGA package.
Hi Jason
It is possible to dowload a new library from the website of Cadsoft.
By Antonino
Yes - I was about to index the 5.8 libraries this weekend, but last night I saw that 5.9 had come out, so I'll need to do that version instead 
It's a matter of copying the files over to my server, and then running a program that indexes all the information into a database which can then be queried from the web.
It can do any library (and also tell the user where they can download that library from [i.e.a library source]) - I've also indexed the SparkFun library - but the CadSoft FTP libraries really do need a bit of a clean: there's multiple versions of the same one, often with a comment to say that they added another component, or corrected a different one. Theoretically, this should retire the older versions, but they're still there...
I've also released the libraries for most of the components I've had to use, and have indexed them too (although they're not in the current index).
I don't really have any particular problem with the site; I rarely use the libraries that are there, and I'm happy to generate my own.
I was initially just saying that I've done an extensive search in the standard libraries for those footprints, and couldn't find any. The current Eagle search is a bit limiting (it's very easy to miss what you're looking for), and I've written my own search capabilities (Richard is aware of this; it was posted in another topic).
I don't really have any particular problem with the site; I rarely use the libraries that are there, and I'm happy to generate my own.
I was initially just saying that I've done an extensive search in the standard libraries for those footprints, and couldn't find any. The current Eagle search is a bit limiting (it's very easy to miss what you're looking for), and I've written my own search capabilities (Richard is aware of this; it was posted in another topic).