Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to get a better display when use "show" command highlight a wire or a part?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 190 subscribers
  • Views 1973 views
  • Users 0 members are here
Related

How to get a better display when use "show" command highlight a wire or a part?

huayuliang
huayuliang over 16 years ago

Hello!

 

In the schematic editor of EAGLE, "show"  is one of most commonly used commands, but it is not very clear when a wire or a part that be highligt or not highligt.

 

how to set colors can get better effect ?

 

someone think if it can be flash on highlight object would be better. maybe it is difficult for eagle .

 

在使用 show 命令时,原理图中元件、连线的高亮对比并不明显,如何设置可以得到明显的对比效果呢?

 

当然,如果能够使show的对象闪烁最好。

  • Sign in to reply
  • Cancel
Parents
  • Michael
    0 Michael over 16 years ago
    Making an object flash when it is highlighted by command SHOW? It's really a good idea, but it seems EAGLE does not support it, I think you need a ULP to make that function happen.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • huayuliang
    0 huayuliang over 16 years ago in reply to Michael

    use ULP can implement this ? could you give me more tips?

     

    show and not show ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to huayuliang

    As of now, I don't think it is possible to highlight different nets with different colors or even change the colors what EAGLE highlights with. In an ULP, you can use only the show command which will again use the standard colors for highlighting. If you need to highlight an entire class of nets, there is an ULP called "showclass.ulp" which highlights the nets belonging to a certain class.

         Probably you could play around with the  black/white background in the schematic or board. For example: the highlighted nets show up much brighter on a white background than a black one on the board.

     

    Best Regards,

    Jaya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to huayuliang

    As of now, I don't think it is possible to highlight different nets with different colors or even change the colors what EAGLE highlights with. In an ULP, you can use only the show command which will again use the standard colors for highlighting. If you need to highlight an entire class of nets, there is an ULP called "showclass.ulp" which highlights the nets belonging to a certain class.

         Probably you could play around with the  black/white background in the schematic or board. For example: the highlighted nets show up much brighter on a white background than a black one on the board.

     

    Best Regards,

    Jaya