Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to get a better display when use "show" command highlight a wire or a part?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2092 views
  • Users 0 members are here
Related

How to get a better display when use "show" command highlight a wire or a part?

huayuliang
huayuliang over 16 years ago

Hello!

 

In the schematic editor of EAGLE, "show"  is one of most commonly used commands, but it is not very clear when a wire or a part that be highligt or not highligt.

 

how to set colors can get better effect ?

 

someone think if it can be flash on highlight object would be better. maybe it is difficult for eagle .

 

在使用 show 命令时,原理图中元件、连线的高亮对比并不明显,如何设置可以得到明显的对比效果呢?

 

当然,如果能够使show的对象闪烁最好。

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 16 years ago

    Hello,

     

    you could either use the SHOW command with the @ option in order to find an object, or you could define a bright highlight color. The SHOW command can look like this:  SHOW @ IC1   In this case EAGLE will draw a pointer to the object and draw a rectangle around it.

    For defining another highlight color go to the Options/Set/Color menu and change the color settings. For details please take a look into the EAGLE manual, chapter 5, Color Settings.

     

    Hope this helps.

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Michael
    0 Michael over 16 years ago in reply to Richard_H
    Yes, EAGLE can also do this way.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Michael
    0 Michael over 16 years ago in reply to Richard_H
    Yes, EAGLE can also do this way.