Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum How to get a better display when use "show" command highlight a wire or a part?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2092 views
  • Users 0 members are here
Related

How to get a better display when use "show" command highlight a wire or a part?

huayuliang
huayuliang over 16 years ago

Hello!

 

In the schematic editor of EAGLE, "show"  is one of most commonly used commands, but it is not very clear when a wire or a part that be highligt or not highligt.

 

how to set colors can get better effect ?

 

someone think if it can be flash on highlight object would be better. maybe it is difficult for eagle .

 

在使用 show 命令时,原理图中元件、连线的高亮对比并不明显,如何设置可以得到明显的对比效果呢?

 

当然,如果能够使show的对象闪烁最好。

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 16 years ago

    Hello,

     

    you could either use the SHOW command with the @ option in order to find an object, or you could define a bright highlight color. The SHOW command can look like this:  SHOW @ IC1   In this case EAGLE will draw a pointer to the object and draw a rectangle around it.

    For defining another highlight color go to the Options/Set/Color menu and change the color settings. For details please take a look into the EAGLE manual, chapter 5, Color Settings.

     

    Hope this helps.

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • huayuliang
    0 huayuliang over 16 years ago in reply to Richard_H

    maybe I didn't explain my real means, sorry.

     

    I want show a wire or net or component between the board editor and schematic editor. do not to find some element.

     

    In board editor, all is ok, because I use black color background; but in schematic editor, I use white color as backgound, so the highligh isn't easy to view, contrast is not strong.

     

    I am not good in the color selection, not have vision problem image

     

     

    btw, since often check between the schematic and board,  once I switch different sheet of schematic, the SHOW command will stop. I feel here is a bad operating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to huayuliang

    Yes, Once you switch between various sheets of a schematic, the "show" command is deactivated. But if you highlight a certain net on the board first and then switch to the schematic the "show" command is still active,  and the same nets shows highlighted on the schematic too, provided you have both the windows opened. But, doesn't work vice versa that is,  if you highlight a net on the schematic first and then switch to the Board, the show command gets deactivated.

     

    BR-

    Jaya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Michael

    may be not. will let CadSoft know.

     

    -Jaya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Michael
    0 Michael over 16 years ago in reply to e14 Contributor
    So I don't understant why EAGLE "doesn't vice versa"....Is it way too difficult to realize in the software?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Michael
    0 Michael over 16 years ago in reply to e14 Contributor
    So I don't understant why EAGLE "doesn't vice versa"....Is it way too difficult to realize in the software?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Michael

    may be not. will let CadSoft know.

     

    -Jaya